<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EIM bus access serialized across cores? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370123#M52809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an application that uses the EIM bus to communicate with and FPGA.&lt;/P&gt;&lt;P&gt;There is an additional device connected to the FPGA, which communicates through the fpga by means of the EIM bus,&lt;/P&gt;&lt;P&gt;and has its own interrupts.&lt;/P&gt;&lt;P&gt;There is also a userspace program accessing registers via the EIM bus, which has been mmapped for direct access.&lt;/P&gt;&lt;P&gt;Thats a driver, two irqs, and a threaded application that may all be trying to read or write the EIM bus. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was not my design, but I am wondering: does the IMX.6 serialize access to the EIM Bus, or do I have a race condition?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Apr 2015 15:54:58 GMT</pubDate>
    <dc:creator>joshuaclayton</dc:creator>
    <dc:date>2015-04-01T15:54:58Z</dc:date>
    <item>
      <title>EIM bus access serialized across cores?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370123#M52809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an application that uses the EIM bus to communicate with and FPGA.&lt;/P&gt;&lt;P&gt;There is an additional device connected to the FPGA, which communicates through the fpga by means of the EIM bus,&lt;/P&gt;&lt;P&gt;and has its own interrupts.&lt;/P&gt;&lt;P&gt;There is also a userspace program accessing registers via the EIM bus, which has been mmapped for direct access.&lt;/P&gt;&lt;P&gt;Thats a driver, two irqs, and a threaded application that may all be trying to read or write the EIM bus. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was not my design, but I am wondering: does the IMX.6 serialize access to the EIM Bus, or do I have a race condition?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2015 15:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370123#M52809</guid>
      <dc:creator>joshuaclayton</dc:creator>
      <dc:date>2015-04-01T15:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: EIM bus access serialized across cores?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370124#M52810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EIM module is connected with AXI bus, allowing processing&lt;/P&gt;&lt;P&gt;one master at time, as described in &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt;&amp;nbsp; sect.22.1.1 Features:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ARM AXI slave interface. One ID at a time support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 09:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370124#M52810</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-02T09:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: EIM bus access serialized across cores?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370125#M52811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Igor.&lt;/P&gt;&lt;P&gt;I could not have possibly comprehended the contents of the reference manual without knowing to go look up AXI in ARM documentation. Well, thats one less item to worry about.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 23:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-bus-access-serialized-across-cores/m-p/370125#M52811</guid>
      <dc:creator>joshuaclayton</dc:creator>
      <dc:date>2015-04-02T23:30:14Z</dc:date>
    </item>
  </channel>
</rss>