<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.Mx6 SoloLite BootStrap in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369868#M52779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.3333330154419px;"&gt;I understand that isolation buffers are necessary when the Boot signals are muxed to be used for some other interface as well (say interfacing a LCD to the processor).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"If &lt;STRONG&gt;not using the boot signals&lt;/STRONG&gt; (LCD_DAT0 - LCD_DAT23) for any other interface, in that case can we avoid the isolation buffers?"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Apr 2015 06:33:48 GMT</pubDate>
    <dc:creator>pankajrana</dc:creator>
    <dc:date>2015-04-02T06:33:48Z</dc:date>
    <item>
      <title>i.Mx6 SoloLite BootStrap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369866#M52777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Referring to the MCIMX6SLEVK schematics, can we remove the ICs U21,U22,U23 and U31 circuitry if not using LCD signals for any other purpose other than Booting ?&lt;/P&gt;&lt;P&gt;I believe we can directly connect the BT_CFG nets to the 4.7KOhm resistors, will it cause any harm ? please comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2015 14:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369866#M52777</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2015-04-01T14:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6 SoloLite BootStrap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369867#M52778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp; From Table 1-2 (EIM recommendations for developer’s boot modes)&lt;BR /&gt; of the Hardware Development Guide for i.MX 6SoloLite :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;“Isolation buffers are required because 6SoloLite pads&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;can be set to 1.8V or 3V logic levels while boot signals&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;require 3V logic level to latch the boot settings.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Any pull-ups for boot configuration line must be properly&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;isolated because there is a chance that the system may&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;use 1.8V logic levels.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 06:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369867#M52778</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-02T06:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6 SoloLite BootStrap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369868#M52779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.3333330154419px;"&gt;I understand that isolation buffers are necessary when the Boot signals are muxed to be used for some other interface as well (say interfacing a LCD to the processor).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"If &lt;STRONG&gt;not using the boot signals&lt;/STRONG&gt; (LCD_DAT0 - LCD_DAT23) for any other interface, in that case can we avoid the isolation buffers?"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 06:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369868#M52779</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2015-04-02T06:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6 SoloLite BootStrap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369869#M52780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2015 08:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-SoloLite-BootStrap/m-p/369869#M52780</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-03T08:13:43Z</dc:date>
    </item>
  </channel>
</rss>