<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 SDMA performance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SDMA-performance/m-p/369614#M52721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;40-60 MB/s is typical figure, so it can not be considered&lt;/P&gt;&lt;P&gt;as abnormal. Probably you can try to decrease number of running&lt;/P&gt;&lt;P&gt;applications, if possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Feb 2015 08:35:38 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-02-12T08:35:38Z</dc:date>
    <item>
      <title>i.MX6 SDMA performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SDMA-performance/m-p/369613#M52720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We applyed old i.MX6 ltib SDMA:ap_2_ap patch for yocto then it worked.&lt;BR /&gt;However, the performance is not enough for us. It was under 40MB/s. &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(Please refer to &lt;/SPAN&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="353963" data-objecttype="2" href="https://community.freescale.com/message/353963#353963"&gt;https://community.freescale.com/message/353963#353963&lt;/A&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do we have any way to improve the performance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 06:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SDMA-performance/m-p/369613#M52720</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2015-02-12T06:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 SDMA performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SDMA-performance/m-p/369614#M52721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;40-60 MB/s is typical figure, so it can not be considered&lt;/P&gt;&lt;P&gt;as abnormal. Probably you can try to decrease number of running&lt;/P&gt;&lt;P&gt;applications, if possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 08:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SDMA-performance/m-p/369614#M52721</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-12T08:35:38Z</dc:date>
    </item>
  </channel>
</rss>