<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using USB device without VDD5V on imX28 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-USB-device-without-VDD5V-on-imX28/m-p/369242#M52648</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid there are no such patches for WinCE60.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Apr 2015 00:46:15 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-04-07T00:46:15Z</dc:date>
    <item>
      <title>Using USB device without VDD5V on imX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-USB-device-without-VDD5V-on-imX28/m-p/369241#M52647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use the USB OTG Port in device only mode without having VDD5V present. I have seen that there is a patch for Linux L2.6.35_1.1.0 (&lt;A href="https://community.nxp.com/message/470993"&gt;USB Device not work when VDD5V is not attached during boot (iMX28)).&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Is there a similar patch for windows CE 6.0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2015 07:35:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-USB-device-without-VDD5V-on-imX28/m-p/369241#M52647</guid>
      <dc:creator>MartinHo</dc:creator>
      <dc:date>2015-04-01T07:35:37Z</dc:date>
    </item>
    <item>
      <title>Re: Using USB device without VDD5V on imX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-USB-device-without-VDD5V-on-imX28/m-p/369242#M52648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid there are no such patches for WinCE60.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 00:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-USB-device-without-VDD5V-on-imX28/m-p/369242#M52648</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-07T00:46:15Z</dc:date>
    </item>
  </channel>
</rss>