<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem in running the samples from gpu_sdk_v1.00 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369202#M52644</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;update&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am running on lxde(3.10.17 linux image from Boundary devices). I was getting that error because i was trying to compile the samples from the serial console on my pc connected from the board but when i try from a terminal window from the device itself, the "bin" directory is created and the binaries are present inside it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But,when i try to run a binary, it gives the following message on the screen&lt;/P&gt;&lt;P&gt;./01_SimpleTriangle&lt;/P&gt;&lt;P&gt;Lesson 02&lt;/P&gt;&lt;P&gt;chooseconfig,&lt;/P&gt;&lt;P&gt;createwindow,&lt;/P&gt;&lt;P&gt;createcontext,&lt;/P&gt;&lt;P&gt;makecurrent,&lt;/P&gt;&lt;P&gt;exiting init,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then it waits and no response till i forcefully interrupt it.&lt;/P&gt;&lt;P&gt;Can someone help me with it??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sudlin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Jan 2015 08:02:36 GMT</pubDate>
    <dc:creator>sudiptasubudhi</dc:creator>
    <dc:date>2015-01-30T08:02:36Z</dc:date>
    <item>
      <title>Problem in running the samples from gpu_sdk_v1.00</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369200#M52642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to port gpu_sdk_v1.00 obtained from freescale onto Nitrogen6x board (IMX6) and run the samples provided by the sdk. I am using ubuntu 14.04 image.I am compiling on target using fbdev. After compilation,the "bin" directory is not generated automatically but the binaries of the samples are created in their respective folders. when i am trying to run any one of them,it is giving an error:&lt;/P&gt;&lt;P&gt;root@nitrogen:/sdk/Samples/GLES1.1/01_SimpleTriangle# ./01_SimpleTriangle&lt;/P&gt;&lt;P&gt;Lesson 02&lt;/P&gt;&lt;P&gt;./01_SimpleTriangle: symbol lookup error: ./01_SimpleTriangle: undefined symbol: fbGetDisplayByIndex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, how to get out of it ? Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sudlin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 13:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369200#M52642</guid>
      <dc:creator>sudiptasubudhi</dc:creator>
      <dc:date>2015-01-22T13:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in running the samples from gpu_sdk_v1.00</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369201#M52643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/space/11067"&gt;Boundary Devices&lt;/A&gt; do you have information to help Sudlin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2015 18:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369201#M52643</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-01-27T18:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in running the samples from gpu_sdk_v1.00</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369202#M52644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;update&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am running on lxde(3.10.17 linux image from Boundary devices). I was getting that error because i was trying to compile the samples from the serial console on my pc connected from the board but when i try from a terminal window from the device itself, the "bin" directory is created and the binaries are present inside it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But,when i try to run a binary, it gives the following message on the screen&lt;/P&gt;&lt;P&gt;./01_SimpleTriangle&lt;/P&gt;&lt;P&gt;Lesson 02&lt;/P&gt;&lt;P&gt;chooseconfig,&lt;/P&gt;&lt;P&gt;createwindow,&lt;/P&gt;&lt;P&gt;createcontext,&lt;/P&gt;&lt;P&gt;makecurrent,&lt;/P&gt;&lt;P&gt;exiting init,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then it waits and no response till i forcefully interrupt it.&lt;/P&gt;&lt;P&gt;Can someone help me with it??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sudlin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 08:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369202#M52644</guid>
      <dc:creator>sudiptasubudhi</dc:creator>
      <dc:date>2015-01-30T08:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in running the samples from gpu_sdk_v1.00</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369203#M52645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;The Problem got solved.The mistake i was doing is i was using the lxde image provided by Boundary devices which has X support. As i was compiling using fbdev windowing system the console image provided by the Boundary devices works well and the freescale gpu sdk samples are running on 3.10.17 kernel.&lt;/P&gt;&lt;P&gt;These are the requirements if you are using a Nitrogen6x board and 3.10.17 kernel:&lt;/P&gt;&lt;P&gt;1. Rootfs :&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="http://boundarydevices.com/eula?file=20141215-nitrogen-3.10.17_1.0.2_ga-trusty-en_US-console_armhf.img.gz" style="color: #154096;"&gt;20141215-nitrogen-3.10.17_1.0.2_ga-trusty-en_US-console_armhf.img.gz&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; available at&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://boundarydevices.com/ubuntu-trusty-december-2014-release/"&gt;http://boundarydevices.com/ubuntu-trusty-december-2014-release/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.Install gpu-viv-bin-mx6q-1.10.17-1.0.0.tar.gz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.Install the following packages:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; available at timesys&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i) linux-libc-dev-armhf-cross_3.13.0-12.32cross1.104_all.deb&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ii) libc6-armhf-cross_2.19-0ubuntu2cross1.104_all.deb&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; iii) libc6-dev-armhf-cross_2.19-0ubuntu2cross1.104_all.deb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.Then follow the instructions provided in the pdf present in the freescale gpu_sdk for the symlinks required for the libraries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sudlin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 07:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369203#M52645</guid>
      <dc:creator>sudiptasubudhi</dc:creator>
      <dc:date>2015-02-03T07:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in running the samples from gpu_sdk_v1.00</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369204#M52646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for posting the solution Sudlin!, it will help other users in the future!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Feb 2015 18:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-running-the-samples-from-gpu-sdk-v1-00/m-p/369204#M52646</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-02-19T18:43:56Z</dc:date>
    </item>
  </channel>
</rss>