<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Graphics on iMX6Solo using mainline kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369040#M52626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Starting with our recent 3.10.53-1.1.0 GA release that just came out it is possible to mix and match kernels starting this release (but with graphics from previous releases like 3.10.17).&amp;nbsp; We separated out the&amp;nbsp; graphics kernel driver into a loadable module.&amp;nbsp; Now we made this change so customers in future would have ability to mix and match graphics releases with other kernels (only starting with 3.10.53) but did not consider it being used for community kernels.&amp;nbsp; However it should&amp;nbsp; work - we've just not tried it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jan 2015 15:52:22 GMT</pubDate>
    <dc:creator>LaurenPost</dc:creator>
    <dc:date>2015-01-22T15:52:22Z</dc:date>
    <item>
      <title>Graphics on iMX6Solo using mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369039#M52625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use accelerated graphics on iMX6Solo with the current mainline (3.19 RC) kernel? If yes then what have to be done to get it working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Matthias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 13:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369039#M52625</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2015-01-22T13:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: Graphics on iMX6Solo using mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369040#M52626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Starting with our recent 3.10.53-1.1.0 GA release that just came out it is possible to mix and match kernels starting this release (but with graphics from previous releases like 3.10.17).&amp;nbsp; We separated out the&amp;nbsp; graphics kernel driver into a loadable module.&amp;nbsp; Now we made this change so customers in future would have ability to mix and match graphics releases with other kernels (only starting with 3.10.53) but did not consider it being used for community kernels.&amp;nbsp; However it should&amp;nbsp; work - we've just not tried it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 15:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369040#M52626</guid>
      <dc:creator>LaurenPost</dc:creator>
      <dc:date>2015-01-22T15:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: Graphics on iMX6Solo using mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369041#M52627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer. And sorry for asking a dumb question again: Where can I download that release? I can only find something called L3.10.17_1.0.0_IMX6QDLS_BUNDLE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 08:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Graphics-on-iMX6Solo-using-mainline-kernel/m-p/369041#M52627</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2015-01-23T08:53:40Z</dc:date>
    </item>
  </channel>
</rss>