<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGUI does not start when enabling GPU profiling from kernel command line</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GUI-does-not-start-when-enabling-GPU-profiling-from-kernel/m-p/369019#M52623</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using kernel 3.10.17 with yocto rootfs. The kernel is built with CONFIG_MXC_GPU_VIV=y.&lt;/P&gt;&lt;P&gt;When I add "gpuProfiler=1" to the kernel command line, then the yocto qt GUI won't start.&lt;/P&gt;&lt;P&gt;Do I miss something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Mar 2015 10:29:29 GMT</pubDate>
    <dc:creator>oussama</dc:creator>
    <dc:date>2015-03-09T10:29:29Z</dc:date>
    <item>
      <title>GUI does not start when enabling GPU profiling from kernel command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GUI-does-not-start-when-enabling-GPU-profiling-from-kernel/m-p/369019#M52623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using kernel 3.10.17 with yocto rootfs. The kernel is built with CONFIG_MXC_GPU_VIV=y.&lt;/P&gt;&lt;P&gt;When I add "gpuProfiler=1" to the kernel command line, then the yocto qt GUI won't start.&lt;/P&gt;&lt;P&gt;Do I miss something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2015 10:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GUI-does-not-start-when-enabling-GPU-profiling-from-kernel/m-p/369019#M52623</guid>
      <dc:creator>oussama</dc:creator>
      <dc:date>2015-03-09T10:29:29Z</dc:date>
    </item>
    <item>
      <title>Re: GUI does not start when enabling GPU profiling from kernel command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GUI-does-not-start-when-enabling-GPU-profiling-from-kernel/m-p/369020#M52624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi oussama,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vprofiler does not work properly on 3.10.17 and X11 - QT yocto backends, you should try the 3.10.53 kernel base that includes the 5.0.11p1 Vivante driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Alfredo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2015 16:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GUI-does-not-start-when-enabling-GPU-profiling-from-kernel/m-p/369020#M52624</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-03-10T16:13:56Z</dc:date>
    </item>
  </channel>
</rss>