<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX280 : Input leakage Current</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX280-Input-leakage-Current/m-p/368640#M52525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Nov 2014 03:15:14 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2014-11-28T03:15:14Z</dc:date>
    <item>
      <title>iMX280 : Input leakage Current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX280-Input-leakage-Current/m-p/368639#M52524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the i.MX28 Data Sheet (IMX23CEC Rev3) .&lt;BR /&gt;However, I can not find an Input leakage Current value .&lt;/P&gt;&lt;P&gt;How much is the Input leakage Current value ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2014 10:10:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX280-Input-leakage-Current/m-p/368639#M52524</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2014-11-25T10:10:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX280 : Input leakage Current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX280-Input-leakage-Current/m-p/368640#M52525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 03:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX280-Input-leakage-Current/m-p/368640#M52525</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2014-11-28T03:15:14Z</dc:date>
    </item>
  </channel>
</rss>