<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSDIO/MMC v2/3 Host Throughput</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368611#M52518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum effective throughput that could be achieved in the SD/MNC host controller for the various IMX series of processors (IMX 3/5/6) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any test suite for EVK or respective factory profiled value for the various platforms along with its associated scenarios ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Nov 2014 10:06:47 GMT</pubDate>
    <dc:creator>lyfsci</dc:creator>
    <dc:date>2014-11-25T10:06:47Z</dc:date>
    <item>
      <title>SDIO/MMC v2/3 Host Throughput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368611#M52518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum effective throughput that could be achieved in the SD/MNC host controller for the various IMX series of processors (IMX 3/5/6) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any test suite for EVK or respective factory profiled value for the various platforms along with its associated scenarios ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2014 10:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368611#M52518</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2014-11-25T10:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO/MMC v2/3 Host Throughput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368612#M52519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SD/MMC controller cores of the i.MX3x and i.MX5x series processors are pretty similar. They support the SD/SDIO v.2.0 specification and MMC v.4.2 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;— Card bus clock frequency up to 52 MHz&lt;/P&gt;&lt;P&gt;— Up to 416 Mbits/s of data transfer for MMC cards in 8-bit mode&lt;/P&gt;&lt;P&gt;— Up to 200 Mbits/s of data transfer for SD/SDIO cards in 4-bit mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SD/MMC controller cores of the i.MX6x series processors support the SD/SDIO v.3.0 specification and MMC v.4.41 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bus clock frequencies supported are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- MMC full speed mode (up to 20 MHz)&lt;/P&gt;&lt;P&gt;- MMC high speed mode (up to 52 MHz)&lt;/P&gt;&lt;P&gt;- MMC DDR mode (52MHz both edges)&lt;/P&gt;&lt;P&gt;- SD/SDIO full speed mode (up to 25 MHz)&lt;/P&gt;&lt;P&gt;- SD/SDIO high speed mode (up to 50 MHz)&lt;/P&gt;&lt;P&gt;- SD/SDIO UHS-I mode(up to 208Mhz in SDR mode, up to 50Mhz in DDR mode)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The corresponding data rates are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Up to 832 Mbits/s of data transfer for SD/SDIO cards using 4 parallel data lines in SDR(Single Data Rate) mode&lt;/P&gt;&lt;P&gt;- Up to 400 Mbits/s of data transfer for SD/SDIO card using 4 parallel data lines in DDR(Dual Data Rate) mode&lt;/P&gt;&lt;P&gt;- Up to 832 Mbits/s of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode&lt;/P&gt;&lt;P&gt;- Up to 400 Mbits/s of data transfer for SDXC card using 4 parallel data lines in DDR(Dual Data Rate) mode&lt;/P&gt;&lt;P&gt;- Up to 416 Mbits/s of data transfer for MMC cards using 8 parallel data lines in SDR(Single Data Rate) mode&lt;/P&gt;&lt;P&gt;- Up to 832 Mbits/s of data transfer for MMC cards using 8 parallel data lines in DDR(Dual Data Rate) mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are no dedicated test cases for SD/MMC controller cores speed test, since the real data throughput depends on many factors, such as speed of device connected, software overhead etc.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 02:46:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368612#M52519</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2014-11-28T02:46:21Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO/MMC v2/3 Host Throughput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368613#M52520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The above mentioned items seems to be the ideal throughput value whereas I look for the actual throughput achieved beyond the signaling constraints in the SoC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Nov 2014 07:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/368613#M52520</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2014-11-29T07:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO/MMC v2/3 Host Throughput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/1661161#M206889</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to use the Variscite DART6UL board for a project. It has the NXP i.MX 6 Ultralite ARM Cortex-A7 processor. I need to transfer data at 20MB/sec to a SD card.&lt;/P&gt;&lt;P&gt;Does anyone know if that kind of throughput rate is possible with the SD driver running and managing the file structure and writing operation to the SD FLASH memory?&lt;/P&gt;&lt;P&gt;I am concerned about the overhead the driver will impose on the overall data-rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, am I correct in assuming the data can be moved under DMA from a parallel input port to the SD bus?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 20:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-MMC-v2-3-Host-Throughput/m-p/1661161#M206889</guid>
      <dc:creator>dfasano</dc:creator>
      <dc:date>2023-05-31T20:03:27Z</dc:date>
    </item>
  </channel>
</rss>