<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic core-image-minimal Yocto for imx53qsb in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-Yocto-for-imx53qsb/m-p/368504#M52501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built the image for imx53qsb. I tried to run it on the imx53qsb but It seemed to not work. I used an SDCard to load it but it didn't work. even though I tried with some prebuilt images that I found from the next link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/" title="http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/"&gt;Index of /releases/yocto/yocto-1.6/machines/imx53qsb&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that for testing this build configuration I have to use the rs232 port even though I do not know the settings for connecting the serial port of my pc to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could somebody give me an advice or hints that I should check to get this working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I followed all the instructions given here &lt;A href="https://community.nxp.com/docs/DOC-1616"&gt;Freescale Yocto Project main page&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 05 Oct 2014 22:36:57 GMT</pubDate>
    <dc:creator>luishernandez</dc:creator>
    <dc:date>2014-10-05T22:36:57Z</dc:date>
    <item>
      <title>core-image-minimal Yocto for imx53qsb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-Yocto-for-imx53qsb/m-p/368504#M52501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built the image for imx53qsb. I tried to run it on the imx53qsb but It seemed to not work. I used an SDCard to load it but it didn't work. even though I tried with some prebuilt images that I found from the next link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/" title="http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/"&gt;Index of /releases/yocto/yocto-1.6/machines/imx53qsb&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that for testing this build configuration I have to use the rs232 port even though I do not know the settings for connecting the serial port of my pc to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could somebody give me an advice or hints that I should check to get this working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I followed all the instructions given here &lt;A href="https://community.nxp.com/docs/DOC-1616"&gt;Freescale Yocto Project main page&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Oct 2014 22:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-Yocto-for-imx53qsb/m-p/368504#M52501</guid>
      <dc:creator>luishernandez</dc:creator>
      <dc:date>2014-10-05T22:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: core-image-minimal Yocto for imx53qsb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-Yocto-for-imx53qsb/m-p/368505#M52502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check if the demo image is working on Your board.&lt;BR /&gt;To prepare SD card image :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ sudo dd if=&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;core-image-minimal-dev-imx53qsb.sdcard&lt;/SPAN&gt; of=/dev/sdb bs=1M&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/core-image-minimal-dev-imx53qsb.sdcard"&gt;http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/core-image-minimal-dev-imx53qsb.sdcard&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at the following for some details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Task #4 - Deploy and test"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="94989" data-objecttype="102" href="https://community.freescale.com/docs/DOC-94989"&gt;https://community.freescale.com/docs/DOC-94989&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;As for host PC configuring, please refer to sections 6.1 (Setup Terminal) and &lt;BR /&gt;3.2 (How to Boot From Micro SD Card) of the enclosed "i.MX53_START_Linux_BSP_UserGuide.pdf"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Oct 2014 00:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-Yocto-for-imx53qsb/m-p/368505#M52502</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-06T00:33:36Z</dc:date>
    </item>
  </channel>
</rss>