<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR stress test issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-issue/m-p/367742#M52350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The shown&amp;nbsp; messages relate to interface between internal iROM bootloader of &lt;/P&gt;&lt;P&gt;i.MX6 and an application, that tries to load and run (memory) tests&amp;nbsp; via i.MX6 USB &lt;/P&gt;&lt;P&gt;serial boot mode. There are two possible causes of the issue.&lt;/P&gt;&lt;P&gt;1. The board does not start in the bootstrap (serial download) mode.&lt;/P&gt;&lt;P&gt;2. There is no connection between a PC and the i.MX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jan 2015 08:33:21 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-01-22T08:33:21Z</dc:date>
    <item>
      <title>DDR stress test issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-issue/m-p/367741#M52349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-size: 13.3333339691162px;"&gt;Hi,All&lt;/P&gt;&lt;P style="font-size: 13.3333339691162px;"&gt;The following picture is the operation after DDR stress tool testing:&lt;/P&gt;&lt;P style="font-size: 13.3333339691162px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49050i77EEE624980CB7E0/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.bmp" alt="1.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333339691162px;"&gt;and could you tell me some possible reasons?How to solve these problems?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 08:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-issue/m-p/367741#M52349</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-01-22T08:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: DDR stress test issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-issue/m-p/367742#M52350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The shown&amp;nbsp; messages relate to interface between internal iROM bootloader of &lt;/P&gt;&lt;P&gt;i.MX6 and an application, that tries to load and run (memory) tests&amp;nbsp; via i.MX6 USB &lt;/P&gt;&lt;P&gt;serial boot mode. There are two possible causes of the issue.&lt;/P&gt;&lt;P&gt;1. The board does not start in the bootstrap (serial download) mode.&lt;/P&gt;&lt;P&gt;2. There is no connection between a PC and the i.MX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 08:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-issue/m-p/367742#M52350</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-01-22T08:33:21Z</dc:date>
    </item>
  </channel>
</rss>