<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: The question about  the JTAG_MOD</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367167#M52237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if JTAG function is not used at all you can just leave it unconnected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Sep 2014 06:48:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-09-16T06:48:16Z</dc:date>
    <item>
      <title>The question about  the JTAG_MOD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367164#M52234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45966i323561AEA0917D30/image-size/large?v=v2&amp;amp;px=999" title="JTAG_MOD.png" alt="JTAG_MOD.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;1,As the above table said, if I don't want use JTAG function, should the JTAG_MOD pin be connected with pull-up resistance? what is the resistance ?&lt;/P&gt;&lt;P&gt;2,I also find there are three different JTAG security modes:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mode #1: No Debug-Maximum Security.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mode #2: Secure JTAG-High security.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mode #3: JTAG Enabled-Low security.&lt;/P&gt;&lt;P&gt;I am puzzled about these. I think the JTAG security modes only can be select by burning the related e-fuses if the JTAG_MOD pin is connected to GND.&lt;/P&gt;&lt;P&gt;If we connect the&amp;nbsp; JTAG_MOD pin with pull-up resistance, we can not select the mode. Is my understanding right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't want to use JTAG function, which method will be recommended?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you~!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Sep 2014 11:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367164#M52234</guid>
      <dc:creator>王剑翰</dc:creator>
      <dc:date>2014-09-15T11:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: The question about  the JTAG_MOD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367165#M52235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 王 剑翰 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can connect JTAG_MOD pin to ground if JTAG function&lt;/P&gt;&lt;P&gt;is not used. For bsdl testing JTAG_MOD should be high.&lt;/P&gt;&lt;P&gt;JTAG security modes implies:&lt;/P&gt;&lt;P&gt;No Debug-Maximum Securit - jtag just disabled&lt;/P&gt;&lt;P&gt;Secure JTAG-High security.- access with secret patterns&lt;/P&gt;&lt;P&gt;JTAG Enabled-Low security - usual jtag usage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Sep 2014 11:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367165#M52235</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-15T11:32:43Z</dc:date>
    </item>
    <item>
      <title>Re: The question about  the JTAG_MOD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367166#M52236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;Thank you for your quickly answer.&lt;/P&gt;&lt;P&gt;As the table says, I think connecting JTAG_MOD pin to pull-up resistance is also used for no JTAG debug function. Am I right?&lt;/P&gt;&lt;P&gt;I think the difference between JTAG_MOD=0 and JTAG_MOD=1 is chain length. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45973i850B4C714131FBD0/image-size/large?v=v2&amp;amp;px=999" title="SJC-TAP.jpg" alt="SJC-TAP.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;No matter we set JTAG_MOD=0 or JTAG_MOD=1, the boundary scan test can be used.&lt;/P&gt;&lt;P&gt;So I think there are two method for no JTAG function:&lt;/P&gt;&lt;P&gt;1) Connect JTAG_MOD pin to ground and then burn the related e-fuses to enter No Debug-Maximum Securit mode;&lt;/P&gt;&lt;P&gt;2) Connect JTAG_MOD pin to pull-up resistance, so that we don't need to care the related e-fuses;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Above is my understanding, could you kindly correct me if I am wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Sep 2014 02:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367166#M52236</guid>
      <dc:creator>王剑翰</dc:creator>
      <dc:date>2014-09-16T02:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: The question about  the JTAG_MOD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367167#M52237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if JTAG function is not used at all you can just leave it unconnected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Sep 2014 06:48:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367167#M52237</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-16T06:48:16Z</dc:date>
    </item>
    <item>
      <title>Re: The question about  the JTAG_MOD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367168#M52238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer. I think I understand it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Sep 2014 07:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-question-about-the-JTAG-MOD/m-p/367168#M52238</guid>
      <dc:creator>王剑翰</dc:creator>
      <dc:date>2014-09-16T07:50:18Z</dc:date>
    </item>
  </channel>
</rss>