<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Blinking Phenomenon on kernel booting with u-boot splash screen</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366856#M52153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem is that Linux kernel may use different than Uboot clock scheme&lt;/P&gt;&lt;P&gt;for various modules: for example turn on DVFS, cpu frequency scaling, &lt;/P&gt;&lt;P&gt;for that moving IPU/LDB clocks to other sources (PLLs/PFDs) than Uboot.&lt;/P&gt;&lt;P&gt;Also Linux may use different memory organization, turn on L2 cache,&lt;/P&gt;&lt;P&gt;assign other frame buffers for IPU, for that it can turn off it for assigning new tasks. &lt;/P&gt;&lt;P&gt;So shortly, impelementing such task may require significant efforts for modification&lt;/P&gt;&lt;P&gt;both Uboot and Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jan 2015 09:07:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-22T09:07:42Z</dc:date>
    <item>
      <title>Blinking Phenomenon on kernel booting with u-boot splash screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366854#M52151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I'm using i.MX6Solo, and applied splash screen in u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot splash screen and kernel booting is operating well.&lt;/P&gt;&lt;P&gt;But the blinking phenomenon was occurred in kernel afte applyingthe u-boot splash screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to remove the blinking phenomenon in kernel.&lt;/P&gt;&lt;P&gt;Could you tell me how to remove this phenomenon?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Eric.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 04:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366854#M52151</guid>
      <dc:creator>erickang</dc:creator>
      <dc:date>2015-01-22T04:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: Blinking Phenomenon on kernel booting with u-boot splash screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366855#M52152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think this phenomenon was occurred because kernel initialized LVDS again after initializing LVDS in u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 07:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366855#M52152</guid>
      <dc:creator>erickang</dc:creator>
      <dc:date>2015-01-22T07:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: Blinking Phenomenon on kernel booting with u-boot splash screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366856#M52153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem is that Linux kernel may use different than Uboot clock scheme&lt;/P&gt;&lt;P&gt;for various modules: for example turn on DVFS, cpu frequency scaling, &lt;/P&gt;&lt;P&gt;for that moving IPU/LDB clocks to other sources (PLLs/PFDs) than Uboot.&lt;/P&gt;&lt;P&gt;Also Linux may use different memory organization, turn on L2 cache,&lt;/P&gt;&lt;P&gt;assign other frame buffers for IPU, for that it can turn off it for assigning new tasks. &lt;/P&gt;&lt;P&gt;So shortly, impelementing such task may require significant efforts for modification&lt;/P&gt;&lt;P&gt;both Uboot and Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 09:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Blinking-Phenomenon-on-kernel-booting-with-u-boot-splash-screen/m-p/366856#M52153</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-22T09:07:42Z</dc:date>
    </item>
  </channel>
</rss>