<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: Re: Custom IMX28 board, no boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366825#M52137</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried your patch, but I still cannot get the board I am working on to boot. I added some more debugging to your patch (expanded patch with your changes plus my debug output attached)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the additional debugging, I get the following console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPL: Serial Console Initialised &lt;/P&gt;&lt;P&gt;SPL: Initialising Power Block &lt;/P&gt;&lt;P&gt;SPL:&amp;nbsp;&amp;nbsp; Configured for VDD 5v only (no battery) &lt;/P&gt;&lt;P&gt;SPL: Switching CPU clock to 24MHz XTAL &lt;/P&gt;&lt;P&gt;SPL: Setting auto-restart bit &lt;/P&gt;&lt;P&gt;SPL: Setting VDDD 25mV below DC-DC converters &lt;/P&gt;&lt;P&gt;SPL: Setting VDDA 25mV below DC-DC converters &lt;/P&gt;&lt;P&gt;SPL: Setting VDDIO 25mV below DC-DC converters &lt;/P&gt;&lt;P&gt;SPL: Starting 5v input detection comparator &lt;/P&gt;&lt;P&gt;SPL: Starting battery voltage measurement logic &lt;/P&gt;&lt;P&gt;SPL: Initialisating LRADCSPL: Enabling LRADC battery measurement &lt;/P&gt;&lt;P&gt;SPL: LRADC channel 7 is present - configuring &lt;/P&gt;&lt;P&gt;SPL: Finished configuring LRADC channel 7 &lt;/P&gt;&lt;P&gt;SPL: Configuring power source &lt;/P&gt;&lt;P&gt;SPL: Pre-Configuring power block &lt;/P&gt;&lt;P&gt;SPL: Disabling automatic battery voltage measurements &lt;/P&gt;&lt;P&gt;SPL: Configuring power block to boot from 5V input &lt;/P&gt;&lt;P&gt;SPL: 5V VDD good &lt;/P&gt;&lt;P&gt;SPL: Booting from 5V supply &lt;/P&gt;&lt;P&gt;SPL: Powering up 4P2 regulator &lt;/P&gt;&lt;P&gt;SPL: Configuring common 4P2 regulator params &lt;/P&gt;&lt;P&gt;SPL: Configuring 4P2 VDD5V only regulator params &lt;/P&gt;&lt;P&gt;SPL: Starting 4P2 regulator &lt;/P&gt;&lt;P&gt;SPL: Charging 4P2 capacitor &lt;/P&gt;&lt;P&gt;SPL: Disabling 4P2 DC-DC Input &lt;/P&gt;&lt;P&gt;SPL: Setting 4P2 brownout level &lt;/P&gt;&lt;P&gt;SPL: Ramping up current limit (VDD5V only) &lt;/P&gt;&lt;P&gt;SPL: Switching DC-DC converters to 4P2 &lt;/P&gt;&lt;P&gt;SPL: Enabling 4P2 DC-DC Input &lt;/P&gt;&lt;P&gt;SPL: 4P2 regulator powered-up &lt;/P&gt;&lt;P&gt;SPL: Switching CPU core clock source to PLL &lt;/P&gt;&lt;P&gt;SPL: Clearing CLKCTRL_CLKSEQ_BYPASS_CPU bit &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;&amp;lt; at this point, the board hangs &amp;gt;&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last line of output is in mxs_power_clock2pll() which is called if MXS_VBUS_CURRENT_DRAW is not defined - should I be defining this (I hav no idea what the purpose of it is). This is the only point in the code that MXS_VBUS_CURRENT_DRAW is used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The next line of console output should be: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPL: Switching VDDD to DC-DC converters&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Jan 2015 01:35:04 GMT</pubDate>
    <dc:creator>graemeruss</dc:creator>
    <dc:date>2015-01-19T01:35:04Z</dc:date>
    <item>
      <title>Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366764#M52076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I design my own board with an imx28 CPU. I configured the board (resistors on LCD_D0 to LCD_05) to boot on SSP0 (SD card).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to boot without SD card connected, I have the 0x8020a014 error code on the debug console. So it seems it want to boot on Sd card. So it's good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I connect the SD card, I have absolutely nothing on the debug console. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I measured voltage and everything is good except VDD4P2. It equal to 0.8V !!!!! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the schematic :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46412iFF04441C8C005983/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG.png" alt="Capture.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 13:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366764#M52076</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-10-30T13:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366765#M52077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; Please look at my comments below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; The problem may be concerned with the low available current from internal i.MX28 &lt;BR /&gt; regulators in default (start) configuration. This may take place when external parts &lt;BR /&gt; (say, DDR) are fed from i.MX28 PMU. Perhaps it makes sense to test the&amp;nbsp; board (only) &lt;BR /&gt; with i.MX28 (+ minimal USB) mounted.&lt;BR /&gt; &lt;BR /&gt; You may try connecting a diode between VDD5V main and the DCDC_BATT/BATTERY signals, &lt;BR /&gt;this made the power supply stabilized. If this approach will be tested - please pay &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;attention on maximum allowed voltage on the BATTERY pin (4.2 V).&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; The cod 0x8020A014 means ERROR_DDI_SD_MMC_DEVICE_NOT_SUPPORTED, &lt;BR /&gt;that is, the device is not supported, or the device cannot be seen.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Perhaps, the SSP_SCK Polarity issue in ROM also takes place here. &lt;BR /&gt;Instability in SD read may cause the error. Special patch for this issue &lt;BR /&gt;should be applied.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 07:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366765#M52077</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-31T07:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366766#M52078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, I don't have the possibility to connecting a Diode because I use small SMD package so it will be very difficult.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the error code only when the SD card is not in place. So, I think that means Bootmode is well define on SSP0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the reference Design from APF28. If I use the APF28 instead of my own CPU board, everything works fine and the only difference is the CPU power : See the AP28 : schematic below :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46281i018413075DE615A6/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG.png" alt="Capture.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the rest is the same between my own board :&lt;/P&gt;&lt;P&gt;Same U-Boot, same Kernel, same rootfs, same schematic (except power circuit).Is not the same RAM memory but it's 100% pin to pin compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible that the problem comes from the imx-bootlets configuration ? I didn't set the config to VDD5V only because I use Yocto and I don't know how to do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 08:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366766#M52078</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-10-31T08:24:05Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366767#M52079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you try to boot from usb with mxsldr ?&lt;/P&gt;&lt;P&gt;In the errata document for imx28 ( &lt;A href="http://cache.freescale.com/files/32bit/doc/errata/IMX28CE.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/32bit/doc/errata/IMX28CE.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.freescale.com/files/32bit/doc/errata/IMX28CE.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=p…&lt;/A&gt; ) you can see that there is and hardware bug for the boor from an SD card. During my test, I saw that same SD card work and some other don't. So, you can try with another kind of SD card.&lt;/P&gt;&lt;P&gt;Did you measure the current from your power supply and the voltage on LCD0...5 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 08:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366767#M52079</guid>
      <dc:creator>victorien</dc:creator>
      <dc:date>2014-10-31T08:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366768#M52080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current consumtion is 1 mA and the voltage on LCD0..5 is :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LCD0 : 3.14V&lt;/P&gt;&lt;P&gt;LCD1 : 0V&lt;/P&gt;&lt;P&gt;LCD2 : 0V&lt;/P&gt;&lt;P&gt;LCD3 : 3.14V&lt;/P&gt;&lt;P&gt;LCD4 : 0V&lt;/P&gt;&lt;P&gt;LCD5 : 0V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't try with mxsldr because I didn't route USB OTG on my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 09:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366768#M52080</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-10-31T09:48:43Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366769#M52081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The current of 1mA is strange if your board is supplied by 5V power. On my board the current is between 120 and 180 mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another question ; did you generate your bootloader with HAB mode or not ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 10:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366769#M52081</guid>
      <dc:creator>victorien</dc:creator>
      <dc:date>2014-10-31T10:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366770#M52082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think it don't start the 4V2 regulator at all. It's why I have 1mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use Yocto (with bitbake) but I'm not familiar with it so I don't know what is HAB mode and how to generate bootloader with it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 10:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366770#M52082</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-10-31T10:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366771#M52083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't work with Yocto, so I don't know but somewhere there is a script u-boot.bd or u-boot_ivt.bd (if you use uboot). And when you program your sd card you write &lt;EM&gt;sudo dd if=header.bin of=/dev/sdX1 ibs=512 conv=sync &lt;/EM&gt;before your bootloader&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 13:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366771#M52083</guid>
      <dc:creator>victorien</dc:creator>
      <dc:date>2014-10-31T13:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366772#M52084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I don't have this u-boot.bd or u-boot_ivt.db. Neither the header.bin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 08:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366772#M52084</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-06T08:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366773#M52085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Damien, good day !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Your configuration meets the app note AN4199 (Figure 9. Hardware connections for VDD5V-only applications).&lt;BR /&gt; According to the section "Limitations" under the Figure :&lt;BR /&gt;"During the early stage of device startup, before on-chip ROM execution, the input current on&lt;/P&gt;&lt;P&gt;VDD5V is limited to 100 mA.&lt;/P&gt;&lt;P&gt;The device is running on internal LinRegs on power up, and it needs to wait for the software to set&lt;/P&gt;&lt;P&gt;up the 4P2 rail before switching to the DC-DC converter as the power supply. The output current&lt;/P&gt;&lt;P&gt;from LinRegs is much lower than that of the DC-DC converter.&lt;/P&gt;&lt;P&gt;It is strongly suggested to use the i.MX28 power supply to power the i.MX28 ..."&lt;/P&gt;&lt;P&gt;&amp;nbsp; From section 4.1.2.2 (VDD5V source only: software configuration) :&lt;/P&gt;&lt;P&gt;"For an application that uses the VDD5V source only, NO_DCDC_BATT_SOURCE must be defined on&lt;/P&gt;&lt;P&gt;power_prep.c in the bootlet codes. Additionally, the programmer should ensure that&lt;/P&gt;&lt;P&gt;NO_VDD5V_SOURCE is not defined".&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; Perhaps it makes sense to use the bootlets of the &lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;L2.6.35_1.1.0 release, where such &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;configuration is supported.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;For more information please take a look at the next thread :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;&lt;A href="https://community.nxp.com/thread/328118"&gt;Custom HW based on imx28 unable to boot from linux-3.14 (yocto)&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Nov 2014 03:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366773#M52085</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-11-11T03:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366774#M52086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer. I will try with LTIB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another little question, what is the role of the shottky diode between VDD4P2 and Battery/DCDC_BATT in the reference schematic ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT : &lt;/P&gt;&lt;P&gt;I found on this forum that the problem can come from a bad inductor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the 744025150 from Wurth. Do you think I need to choose another one ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 11:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366774#M52086</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-18T11:31:06Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366775#M52087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried with LTIB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've defined &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;NO_DCDC_BATT_SOURCE an recompile the boot stream.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I've defined MEMORY_TEST in boot_prep.c&lt;/P&gt;&lt;P&gt;and I've blown &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;HW_OCOTP_ROM7 ENABLE_SSP_12MA_DRIVE bit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, when I power up my board, I have the following message continuously on the debug console :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configured for 5v only power source.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Battery powered operation disabled.&lt;/P&gt;&lt;P&gt;Nov 20 201410:49:11&lt;/P&gt;&lt;P&gt;FRAC 0x92925552&lt;/P&gt;&lt;P&gt;memory type is DDR2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wait for ddr ready 1power 0x00820710&lt;/P&gt;&lt;P&gt;Frac 0x92925552&lt;/P&gt;&lt;P&gt;start change cpu freq&lt;/P&gt;&lt;P&gt;hbus 0x00000003&lt;/P&gt;&lt;P&gt;cpu 0x00010001&lt;/P&gt;&lt;P&gt;start test memory accress&lt;/P&gt;&lt;P&gt;ddr2 0x40000000&lt;/P&gt;&lt;P&gt;finish simple test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Undefined Ins&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 10:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366775#M52087</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-20T10:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366776#M52088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry to post a new answer but someone can help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I plug my sd card in my custom board I have the following on the debug console :&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Configured for 5v only power source.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Battery powered operation disabled.&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Nov 20 201410:49:11&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;FRAC 0x92925552&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;memory type is DDR2&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wait for ddr ready 1power 0x00820710&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Frac 0x92925552&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;start change cpu freq&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;hbus 0x00000003&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;cpu 0x00010001&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;start test memory accress&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;ddr2 0x40000000&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;finish simple test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Undefined Ins&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;If I plug my SD card in IMX28EVK board I have the following on the debug console :&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configured for 5v only power source.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Battery powered operation disabled.&lt;/P&gt;&lt;P&gt;Nov 25 201414:09:42&lt;/P&gt;&lt;P&gt;FRAC 0x92925552&lt;/P&gt;&lt;P&gt;memory type is DDR2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wait for ddr ready 1power 0x00820710&lt;/P&gt;&lt;P&gt;Frac 0x92925552&lt;/P&gt;&lt;P&gt;start change cpu freq&lt;/P&gt;&lt;P&gt;hbus 0x00000003&lt;/P&gt;&lt;P&gt;cpu 0x00010001&lt;/P&gt;&lt;P&gt;start test memory accress&lt;/P&gt;&lt;P&gt;ddr2 0x40000000&lt;/P&gt;&lt;P&gt;finish simple test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Nov 25 2014 - 14:23:15)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale i.MX28 family&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; 454 MHz&lt;/P&gt;&lt;P&gt;BUS:&amp;nbsp;&amp;nbsp; 151 MHz&lt;/P&gt;&lt;P&gt;EMI:&amp;nbsp;&amp;nbsp; 205 MHz&lt;/P&gt;&lt;P&gt;GPMI:&amp;nbsp;&amp;nbsp; 24 MHz&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 128 MB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; IMX_SSP_MMC: 0, IMX_SSP_MMC: 1&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC or MMC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:04:9f:02:09:37&lt;/P&gt;&lt;P&gt;FEC0&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2014 14:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366776#M52088</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-25T14:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366777#M52089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As&amp;nbsp; the shottky diode : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; First, if VDD4P2 may be used as power source for peripheral, such as &lt;/P&gt;&lt;P&gt;backlight, the&amp;nbsp; diode can keep the power available while VDD5V is removed. &lt;/P&gt;&lt;P&gt;&amp;nbsp; Second, if the DCDC power source is switched from the battery to VDD4P2 in &lt;/P&gt;&lt;P&gt;battery charging period, the diode can keep the DCDC power stream continually at &lt;/P&gt;&lt;P&gt;the meantime it is switched back to the battery while VDD5V is removed . &lt;/P&gt;&lt;P&gt;The Schottky diode can be removed if VDD4P2 will not be used continually at the &lt;/P&gt;&lt;P&gt;meantime it is switched back to the battery while VDD5V is removed. The Schottky &lt;/P&gt;&lt;P&gt;diode can be removed if VDD4P2 will not be used as power source of the external &lt;/P&gt;&lt;P&gt;peripherals and the internal DCDC. Any Schottky diode with low forward voltage &lt;/P&gt;&lt;P&gt;and 1A forward current can be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 05:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366777#M52089</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-11-26T05:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366778#M52090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; The "Undefined Ins" message may be caused because of memory bug.&lt;/P&gt;&lt;P&gt;Also the follwoing may be helpful :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/450451"&gt;What does 'Undefined Ins' mean in u-boot?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/379176"&gt;iMX28evk u-boot sd-card -&amp;amp;gt; Undefined Ins&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 06:01:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366778#M52090</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-11-26T06:01:37Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366779#M52091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I followed the tutorial here : &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.denx.de/?p=u-boot.git;a=blob;f=doc/README.mxs;h=ed2e5688562ac1af55a7c6213f5f3eb825e055b8;hb=HEAD" style="font-size: 10pt; line-height: 1.5em;" title="http://git.denx.de/?p=u-boot.git;a=blob;f=doc/README.mxs;h=ed2e5688562ac1af55a7c6213f5f3eb825e055b8;hb=HEAD"&gt;git.denx.de Git - u-boot.git/blob - doc/README.mxs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;with U-boot 2015.01-rc2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the problem still appears.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have HTLLC message on debug console continuously.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also try to blow HAB_DISABLE fuse with BitBurner (saw in a topic on this forum), but the problem was not solved and now I can't unblow this fuse because when I select the IMX28 in "Select device" in Bitburner, the IMX28 is automatically disconnected from my computer. Do you have any idea ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 12:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366779#M52091</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-27T12:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366780#M52092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First thing you need to debug is why VDD4P2 only outputs 0.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest following the VDD4P2 circuitry as in mx28evk or apf28 circuit that you pointed to.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 12:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366780#M52092</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-11-27T12:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366781#M52093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry, I didn't update you about that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since I patched uboot for VDD5V only, all voltages are good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've solid 5V, 3V3 and 1V8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I've the "Undefined ins" message, the imx28 reset and 4V2 fall down (we can see the capacitor discharge curve on the scope).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, when the imx28 restart, 4V2 goes directly to the 4.2V target voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="F0000TEK.BMP.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47663i3624DA8D133E2ED4/image-size/large?v=v2&amp;amp;px=999" role="button" title="F0000TEK.BMP.bmp" alt="F0000TEK.BMP.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 14:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366781#M52093</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-27T14:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366782#M52094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, got it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the next step is to understand why you get "Undefined ins".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This could be due to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Wrong toolchain: for example building with a toolchain for mx6, which is an armv7. That can cause Undefined Ins on a mx28, which is arm926ejs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Incorrect DDR initialization: if your DDR model is not the same as the mx28evk, then you probably need to adapt the DDR settings to match the required ones as per your DDR datasheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 14:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366782#M52094</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-11-27T14:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: Custom IMX28 board, no boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366783#M52095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use : arm-none-linux-gnueabi (generated by yocto) and my U-boot works on the imx28EVK so i think this is not the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But effectively, I didn't use the same DDR (my board is 512Mb and EVK is 128Mb) so it could be the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a tutorial or a procedure to change the ddr settings ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 14:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX28-board-no-boot/m-p/366783#M52095</guid>
      <dc:creator>dgotfroi</dc:creator>
      <dc:date>2014-11-27T14:52:07Z</dc:date>
    </item>
  </channel>
</rss>