<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6DL : How to set the PCIe PHY Reference Clock  source ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365229#M51712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that understanding is correct and&lt;/P&gt;&lt;P&gt;these settings are sufficient for external clock.&lt;/P&gt;&lt;P&gt;Also one can refer to example below &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/316161"&gt;i.MX6Q: Using an external reference for PCIe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Oct 2014 11:07:43 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-10-30T11:07:43Z</dc:date>
    <item>
      <title>iMX6DL : How to set the PCIe PHY Reference Clock  source ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365228#M51711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I consider using i.MX6DL PCIe PHY&lt;BR /&gt;Please see Table 50-1 (p.4455) in IMX6SDLRM (Rev.1).&lt;/P&gt;&lt;P&gt;I hope use the&amp;nbsp; CLK1(In)&amp;nbsp; to "Reference Clock" as a clock source &lt;BR /&gt;with the following setting.&lt;/P&gt;&lt;P&gt;Is my understanding correct ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CCM_ANALOG_PLL_ENETn (pp.909-911)&lt;BR /&gt;&amp;nbsp; ENABLE_100M：0x1&lt;BR /&gt;&amp;nbsp; BYPASS_CLK_SRC：0x1&lt;BR /&gt;&amp;nbsp; BYPASS：0x1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMU_MISC1n (pp.4528-4530)&lt;BR /&gt;&amp;nbsp; LVDSCLK1_IBEN：0x1&lt;BR /&gt;&amp;nbsp; LVDSCLK1_OBEN：0x0&lt;BR /&gt; &lt;BR /&gt;PCIE_PHY_MPLL_ASIC_IN (pp.4470-4471)&lt;BR /&gt;&amp;nbsp; MPLL_MULTIPLIER：0x19&lt;BR /&gt; &lt;BR /&gt;PCIE_PHY_ATEOBRD_STATUS (pp.4474-4475)&lt;BR /&gt;&amp;nbsp; REF_CLKDIV2_IN：0x0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If some adittional setting is required, could you let me know it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 09:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365228#M51711</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2014-10-30T09:11:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DL : How to set the PCIe PHY Reference Clock  source ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365229#M51712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that understanding is correct and&lt;/P&gt;&lt;P&gt;these settings are sufficient for external clock.&lt;/P&gt;&lt;P&gt;Also one can refer to example below &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/316161"&gt;i.MX6Q: Using an external reference for PCIe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 11:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365229#M51712</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-30T11:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DL : How to set the PCIe PHY Reference Clock  source ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365230#M51713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the following setting,&lt;BR /&gt;does the CLK2(out) output the&amp;nbsp; "Reference Clock"&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMU_MISC1n (pp.4528-4530)&lt;BR /&gt;&amp;nbsp; LVDS2_CLK_SEL : 0b01010 (PCIE_REF) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Reference Clock" is defined at &lt;/P&gt;&lt;P&gt; Table 50-1 (p.4455) in IMX6SDLRM (Rev.1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Nov 2014 10:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DL-How-to-set-the-PCIe-PHY-Reference-Clock-source/m-p/365230#M51713</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2014-11-12T10:29:30Z</dc:date>
    </item>
  </channel>
</rss>