<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 Android line-out audio max volume is very low and not really loud in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Android-line-out-audio-max-volume-is-very-low-and-not/m-p/365169#M51710</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is more a hardware limit than a software one,&amp;nbsp; which value of speaker you are connecting to the SGTL 5000, even do it is a line out you need to have an amplifier to get the gain bigger.&amp;nbsp; I am not expert in Android but in Linux you can do it with ALSA Mixer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With amixer, you can change volumes with the ``amixer set'' command. For example, to change the Master volume, you would issue a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;PRE class="jive-pre"&gt;amixer set Master 15 &lt;/PRE&gt;&lt;CODE&gt; &lt;/CODE&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Please note that the names of the elements can be different for different types of sound cards.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Aug 2014 13:28:41 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2014-08-21T13:28:41Z</dc:date>
    <item>
      <title>i.mx6 Android line-out audio max volume is very low and not really loud</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Android-line-out-audio-max-volume-is-very-low-and-not/m-p/365168#M51709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P lang="en-GB"&gt;I have tested audio with various i.mx6 boards with Android: Wandboard Solo, Wandboard Quad, RIoTBoard and Sabre Lite&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P lang="en-GB"&gt;By all of them I enabled the line-out jacks and disabled all other sound devices in the Android kernel_imx.&lt;/P&gt;&lt;P lang="en-GB"&gt;In the Android settings I switch the volume to the very maximum. But on all boards the max sound is not really loud. Comparable to usual taking.&lt;/P&gt;&lt;P lang="en-GB"&gt;&lt;/P&gt;&lt;P lang="en-GB"&gt;I expected a much higher volume since I was thinking that line out has always the same max signal level. If I try the same speakers with PC line-out it is much louder.&lt;/P&gt;&lt;P lang="en-GB"&gt;&lt;/P&gt;&lt;P lang="en-GB"&gt;Is there any way to increase the max volume in Android for the sgtl5000 codec? As said I have access to the Android source so any possible patch would be appreciated,&lt;/P&gt;&lt;P lang="en-GB"&gt;&lt;/P&gt;&lt;P lang="en-GB"&gt;Many Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 19:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Android-line-out-audio-max-volume-is-very-low-and-not/m-p/365168#M51709</guid>
      <dc:creator>luarch</dc:creator>
      <dc:date>2014-08-18T19:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Android line-out audio max volume is very low and not really loud</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Android-line-out-audio-max-volume-is-very-low-and-not/m-p/365169#M51710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is more a hardware limit than a software one,&amp;nbsp; which value of speaker you are connecting to the SGTL 5000, even do it is a line out you need to have an amplifier to get the gain bigger.&amp;nbsp; I am not expert in Android but in Linux you can do it with ALSA Mixer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With amixer, you can change volumes with the ``amixer set'' command. For example, to change the Master volume, you would issue a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;PRE class="jive-pre"&gt;amixer set Master 15 &lt;/PRE&gt;&lt;CODE&gt; &lt;/CODE&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Please note that the names of the elements can be different for different types of sound cards.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Aug 2014 13:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Android-line-out-audio-max-volume-is-very-low-and-not/m-p/365169#M51710</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-08-21T13:28:41Z</dc:date>
    </item>
  </channel>
</rss>