<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GStreamer error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365097#M51687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone help pls? I am very stuck. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 01:35:39 GMT</pubDate>
    <dc:creator>madstrum</dc:creator>
    <dc:date>2014-10-07T01:35:39Z</dc:date>
    <item>
      <title>GStreamer error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365096#M51686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using a CM-FX6 board ... having issues trying to run GStreamer.&lt;/P&gt;&lt;P&gt;I'm trying to get analog tv in via ADV7180 ... what could be the problem here? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@cm-debian:/# gst-launch tvsrc ! autovideosink&lt;/P&gt;&lt;P&gt;MFW_GST_tvsrc_PLUGIN 3.0.7 build on Jul 31 2013 18:18:05.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.7 build on Apr 18 2013 23:22:23.&lt;/P&gt;&lt;P&gt;sensor chip is adv7180_decoderERROR: unrecognized std! ffffff (PAL=ff, NTSC=b000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;should set the input to 1&lt;/P&gt;&lt;P&gt;Pipeline is live and does not need PREROLL ...&lt;/P&gt;&lt;P&gt;Setting pipeline to PLAYING ...&lt;/P&gt;&lt;P&gt;New clock: GstSystemClock&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0: Internal data flow error.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;gstbasesrc.c(2582): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0:&lt;/P&gt;&lt;P&gt;streaming task paused, reason error (-5)&lt;/P&gt;&lt;P&gt;Execution ended after 10005284338 ns.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;Setting pipeline to READY ...&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;root@cm-debian:/# &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;When I do gst-inspect : &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@cm-debian:/# rm ~/.gstreamer-0.10/registry*&lt;/P&gt;&lt;P&gt;root@cm-debian:/# gst-inspect &amp;gt; inspectlog&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:19754): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libgstffmpegscale.so': libswscale.so.2: cannot opy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:19754): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:19754): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed&lt;/P&gt;&lt;P&gt;root@cm-debian:/# find / -name libswscale.so.2&lt;/P&gt;&lt;P&gt;root@cm-debian:/#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 09:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365096#M51686</guid>
      <dc:creator>madstrum</dc:creator>
      <dc:date>2014-10-03T09:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365097#M51687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone help pls? I am very stuck. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 01:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365097#M51687</guid>
      <dc:creator>madstrum</dc:creator>
      <dc:date>2014-10-07T01:35:39Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365098#M51688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'll try again, do only certain cameras work with the imx6 IPU? &lt;/P&gt;&lt;P&gt;I'm trying to interface it to a Sony SNC-RZ30P via analog video in. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 09:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365098#M51688</guid>
      <dc:creator>madstrum</dc:creator>
      <dc:date>2014-10-07T09:22:51Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365099#M51689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following may be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/310042"&gt;iMx6 ,adv7180 and gstreamer&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/428583"&gt;GStreamer Pipeline issue for SII9135/ADV7180 CSI input&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Oct 2014 01:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365099#M51689</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-08T01:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365100#M51690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It turned out to be a hardware error on the base board, apologies. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Oct 2014 02:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-error/m-p/365100#M51690</guid>
      <dc:creator>madstrum</dc:creator>
      <dc:date>2014-10-08T02:53:11Z</dc:date>
    </item>
  </channel>
</rss>