<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LTIB Build: Commad Prompt and Graphics interface is not coming in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Build-Commad-Prompt-and-Graphics-interface-is-not-coming/m-p/169084#M5166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am building the image using LTIB for the first-time for IMX53. I was able to build it successfully after few hickups. But when I finally copied the image to sdcard(UImage, rootfs), i could not see the prompt or graphic interface. could you please tell me what all I am missing. I have attached the boot logs.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Swamy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Sep 2011 06:51:49 GMT</pubDate>
    <dc:creator>Swamy</dc:creator>
    <dc:date>2011-09-08T06:51:49Z</dc:date>
    <item>
      <title>LTIB Build: Commad Prompt and Graphics interface is not coming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Build-Commad-Prompt-and-Graphics-interface-is-not-coming/m-p/169084#M5166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am building the image using LTIB for the first-time for IMX53. I was able to build it successfully after few hickups. But when I finally copied the image to sdcard(UImage, rootfs), i could not see the prompt or graphic interface. could you please tell me what all I am missing. I have attached the boot logs.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Swamy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2011 06:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Build-Commad-Prompt-and-Graphics-interface-is-not-coming/m-p/169084#M5166</guid>
      <dc:creator>Swamy</dc:creator>
      <dc:date>2011-09-08T06:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Build: Commad Prompt and Graphics interface is not coming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Build-Commad-Prompt-and-Graphics-interface-is-not-coming/m-p/169085#M5167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello, What ltib profile are you building? Min, Gnome,.? What bsp version? Have a look to the BSP release notes of the BSP version tou are worwig with. Video commadnd line patameters have changed a little in the last BSPs. only Gnome mobile will init a graphic interface, Can you see Tux on the display at booting up? Best Regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2011 10:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Build-Commad-Prompt-and-Graphics-interface-is-not-coming/m-p/169085#M5167</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2011-09-08T10:00:59Z</dc:date>
    </item>
  </channel>
</rss>