<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX28 Yocto image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364530#M51597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="loading" href="https://community.nxp.com/thread/320106" title="https://community.freescale.com/thread/320106"&gt;https://community.freescale.com/thread/320106&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Oct 2014 09:55:18 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-10-30T09:55:18Z</dc:date>
    <item>
      <title>IMX28 Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364527#M51594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to build imx28 yocto image.&lt;/P&gt;&lt;P&gt;I am able to build yocto image using bitbake as well as hob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't need all packages for the mcimx28evk board. So I want to remove some packages.&lt;/P&gt;&lt;P&gt;Thus I select hob to build yocto image.But hob doesn't produce sdcard image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any method to produce sdcard image using hob?&lt;/P&gt;&lt;P&gt;How to add/remove packages from yocto image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I change kernel configurations?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 07:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364527#M51594</guid>
      <dc:creator>pt</dc:creator>
      <dc:date>2014-10-30T07:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364528#M51595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;write to SD, run dd command&lt;/P&gt;&lt;P&gt;$ sudo dd if=fsl-image-gui-imx28evk-20130417013203.rootfs.sdcard of=/dev/sdf bs=4M&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at below links how customize image&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95059"&gt;Task #6 - Customize the image&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94967"&gt;i.MX Yocto Project: How do I add an existing package to an image?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94874"&gt;i.MX Yocto Project: ltib versus bitbake&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 08:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364528#M51595</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-30T08:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364529#M51596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;So it is not possible to build sdcard image using hob.&lt;/P&gt;&lt;P&gt;I saw kernel-configuration doc - &lt;A href="https://community.nxp.com/docs/DOC-95045"&gt;Task #5 - Kernel&lt;/A&gt;. I have tried that. But fsl-image-gui is not present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;dtsuser@dtsmachine:~/fsl-community-bsp/build$ bitbake fsl-image-gui&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Loading cache: 100% |############################################################################################################| ETA:&amp;nbsp; 00:00:00&lt;/P&gt;&lt;P&gt;Loaded 1829 entries from dependency cache.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ERROR: Nothing PROVIDES 'fsl-image-gui'. Close matches:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; fsl-image-multimedia&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pt AR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 09:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364529#M51596</guid>
      <dc:creator>pt</dc:creator>
      <dc:date>2014-10-30T09:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364530#M51597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="loading" href="https://community.nxp.com/thread/320106" title="https://community.freescale.com/thread/320106"&gt;https://community.freescale.com/thread/320106&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 09:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364530#M51597</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-30T09:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364531#M51598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used this git - &lt;CODE&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.0_ga&lt;BR /&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=dora_3.10.17-1.0.0_GA"&gt;http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/README?h=dora_3.10.17-1.0.0_GA&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am able to run &lt;STRONG&gt;&lt;EM&gt;bitbake fsl-image-gui.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;pt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 04:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-Yocto-image/m-p/364531#M51598</guid>
      <dc:creator>pt</dc:creator>
      <dc:date>2014-10-31T04:43:23Z</dc:date>
    </item>
  </channel>
</rss>