<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 FreeRDP x11 crash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364075#M51504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm trying to compile and run FreeRDP directly on target board (SabreSD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My cmake script:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;cmake -DWITH_PCSC=ON -DWITH_NEON=ON -DWITH_XI=ON -DARM_FP_ABI=hard&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using fsb-community-bsp Dizzy branch. I've tried the kernel 3.10.17-1.0.1 and repo synced to get 3.10.17-1.0.2.&lt;/P&gt;&lt;P&gt;The image generated is core-image-sato and I'm running without problem Qt5 applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It compiles and installs fine but it always crashes after a few seconds of use. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The launch script is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;xfreerdp /u:user /p:pass /gdi:hw /size:1024x768 /bpp:16 /v:192.168.1.175 /cert-ignore +multitouch +gestures&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I begin a control session with RDP the GPU seem to hang and the image freezes. If I run the launch script from console and kill xfreerdp after crash it gives a GPU[0] error when it recovers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Had anyone tried to use FreeRDP with fsl-community-bsp image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Jan 2015 12:35:57 GMT</pubDate>
    <dc:creator>jorgesoria</dc:creator>
    <dc:date>2015-01-21T12:35:57Z</dc:date>
    <item>
      <title>FreeRDP x11 crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364075#M51504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm trying to compile and run FreeRDP directly on target board (SabreSD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My cmake script:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;cmake -DWITH_PCSC=ON -DWITH_NEON=ON -DWITH_XI=ON -DARM_FP_ABI=hard&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using fsb-community-bsp Dizzy branch. I've tried the kernel 3.10.17-1.0.1 and repo synced to get 3.10.17-1.0.2.&lt;/P&gt;&lt;P&gt;The image generated is core-image-sato and I'm running without problem Qt5 applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It compiles and installs fine but it always crashes after a few seconds of use. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The launch script is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;xfreerdp /u:user /p:pass /gdi:hw /size:1024x768 /bpp:16 /v:192.168.1.175 /cert-ignore +multitouch +gestures&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I begin a control session with RDP the GPU seem to hang and the image freezes. If I run the launch script from console and kill xfreerdp after crash it gives a GPU[0] error when it recovers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Had anyone tried to use FreeRDP with fsl-community-bsp image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2015 12:35:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364075#M51504</guid>
      <dc:creator>jorgesoria</dc:creator>
      <dc:date>2015-01-21T12:35:57Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRDP x11 crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364076#M51505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I asked around and no one hastried FreeRDP, have you tried in RDP communities as well?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 20:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364076#M51505</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-01-23T20:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRDP x11 crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364077#M51506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Sergio, I will try to ask there because it's a very specific problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xFreeRDP is strongly x11 dependant, but if I want to use Qt's eglfs platform I think x11 cannot be a DISTRO_FEATURE (Please, correct me if I'm wrong).&lt;/P&gt;&lt;P&gt;Maybe xFreeRDP needs x11 defined as a DISTRO_FEATURE...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I bitbaked another image with DISTRO_FEATURES_append = " opengl x11" and xFreeRDP seems more stable, but I lose eglfs platform in Qt :smileysad:.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea of how to workaround the recipe so I can get an image x11 and eglfs capable?&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2015 15:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364077#M51506</guid>
      <dc:creator>jorgesoria</dc:creator>
      <dc:date>2015-01-27T15:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRDP x11 crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364078#M51507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Crash seems to be solved with xFreeRDP 1.2.5.&lt;/P&gt;&lt;P&gt;Performance improved a lot in 1920x1080 with a higher value of vmalloc in u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 16:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRDP-x11-crash/m-p/364078#M51507</guid>
      <dc:creator>jorgesoria</dc:creator>
      <dc:date>2015-11-25T16:29:36Z</dc:date>
    </item>
  </channel>
</rss>