<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Missing vgCreateImageAMD Symbol in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Missing-vgCreateImageAMD-Symbol/m-p/168980#M5150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;Using i.MX53 Linux BSP 11.09.01 the amd-gpu-bin-mx51-11.09.01.tar.gz provides the OpenGL/EGL/OpenVG.&amp;nbsp; The OpenVG AMD extensions provide access to the raw image buffer to interact with the IPU which we require.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;The issue we're having is vgCreateImageAMD as defined in VG/ext.h has no symbol in any of the libraries provided so we're unable to use it.&amp;nbsp; Wondering if anyone has pointers to an alternative or an updated library package which includes the missing symbols.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;What we're specifically trying to do is use that raw VGImage buffer as a source for the IPU &lt;SPAN style="font-size: 10pt;"&gt;ipu_lib_overlay_param_t-&amp;gt;user_def_paddr.&amp;nbsp; So any pointers to an alternative way to achieve this would also work, though the AMD extensions also allow for a YUV VGImage which is preferred.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Nov 2012 18:14:37 GMT</pubDate>
    <dc:creator>sebastient</dc:creator>
    <dc:date>2012-11-08T18:14:37Z</dc:date>
    <item>
      <title>Missing vgCreateImageAMD Symbol</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Missing-vgCreateImageAMD-Symbol/m-p/168980#M5150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;Using i.MX53 Linux BSP 11.09.01 the amd-gpu-bin-mx51-11.09.01.tar.gz provides the OpenGL/EGL/OpenVG.&amp;nbsp; The OpenVG AMD extensions provide access to the raw image buffer to interact with the IPU which we require.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;The issue we're having is vgCreateImageAMD as defined in VG/ext.h has no symbol in any of the libraries provided so we're unable to use it.&amp;nbsp; Wondering if anyone has pointers to an alternative or an updated library package which includes the missing symbols.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', times;"&gt;What we're specifically trying to do is use that raw VGImage buffer as a source for the IPU &lt;SPAN style="font-size: 10pt;"&gt;ipu_lib_overlay_param_t-&amp;gt;user_def_paddr.&amp;nbsp; So any pointers to an alternative way to achieve this would also work, though the AMD extensions also allow for a YUV VGImage which is preferred.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Nov 2012 18:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Missing-vgCreateImageAMD-Symbol/m-p/168980#M5150</guid>
      <dc:creator>sebastient</dc:creator>
      <dc:date>2012-11-08T18:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Missing vgCreateImageAMD Symbol</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Missing-vgCreateImageAMD-Symbol/m-p/168981#M5151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;this is what I got:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;vgCreateImageAMD is not supported in the vg driver. Also does not support VG_KHR_EGL_image as well. Only option is to use pbuffer surface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Andre&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 17:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Missing-vgCreateImageAMD-Symbol/m-p/168981#M5151</guid>
      <dc:creator>andre_silva</dc:creator>
      <dc:date>2013-01-11T17:01:24Z</dc:date>
    </item>
  </channel>
</rss>