<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Simultaneous firmware upgrade using MfgTools with imx233 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneous-firmware-upgrade-using-MfgTools-with-imx233/m-p/363710#M51452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;i have a question about mfgtools: &lt;/P&gt;&lt;P&gt;is there any way to load one or more devices (imx233) simoultaneously with different profiles using mfgtools?&lt;/P&gt;&lt;P&gt;This question arises from the need to load different encrypted firmwares on different devices in a production environment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Paolo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Feb 2015 14:32:04 GMT</pubDate>
    <dc:creator>paolomartinetti</dc:creator>
    <dc:date>2015-02-10T14:32:04Z</dc:date>
    <item>
      <title>Simultaneous firmware upgrade using MfgTools with imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneous-firmware-upgrade-using-MfgTools-with-imx233/m-p/363710#M51452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;i have a question about mfgtools: &lt;/P&gt;&lt;P&gt;is there any way to load one or more devices (imx233) simoultaneously with different profiles using mfgtools?&lt;/P&gt;&lt;P&gt;This question arises from the need to load different encrypted firmwares on different devices in a production environment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Paolo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2015 14:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneous-firmware-upgrade-using-MfgTools-with-imx233/m-p/363710#M51452</guid>
      <dc:creator>paolomartinetti</dc:creator>
      <dc:date>2015-02-10T14:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneous firmware upgrade using MfgTools with imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneous-firmware-upgrade-using-MfgTools-with-imx233/m-p/363711#M51453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paolo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the Mfgtool operation manual documentation, in case of the latest mfgtool version 4.1v&amp;nbsp; refers that no more than 4 devices are allowed to be connected simultaneously. you need to check this manual according to the version&amp;nbsp; you are using, since previous mfgtools version are able to update firmware, in less than 4 devices&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 16:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneous-firmware-upgrade-using-MfgTools-with-imx233/m-p/363711#M51453</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-02-11T16:26:15Z</dc:date>
    </item>
  </channel>
</rss>