<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question about i.MX6SDL EB804.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-i-MX6SDL-EB804/m-p/363319#M51344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes for i.MX6SDL latest revision 1.2,&lt;/P&gt;&lt;P&gt;so patches for other (1.3, 1.5) are not needed.&lt;/P&gt;&lt;P&gt;Please note that Linux BSP is unified for all i.MX6 processors&lt;/P&gt;&lt;P&gt;so this patch is suggested to apply for providing universal solution&lt;/P&gt;&lt;P&gt;for all i.MX6 processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Aug 2014 05:45:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-18T05:45:56Z</dc:date>
    <item>
      <title>Question about i.MX6SDL EB804.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-i-MX6SDL-EB804/m-p/363318#M51343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6SDL EB804.&lt;/P&gt;&lt;P&gt;Chapter 3.1 says "To ensure that the new chip revision can be read backfrom the chip, the following patch should be applied.".&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.1.0&amp;amp;id=21464af587382ec1841d5fd346eaf359827c6142"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.1.0&amp;amp;id=21464af587382ec1841d5fd346eaf359827c6142&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the above patch, and it adds chip revisions (1.3, 1.4, and 1.5) to BSP.&lt;/P&gt;&lt;P&gt;Then, according to Table 1 of EB804, the i.MX6SDL new silicon revision 1.2 is 0x00000012 in USB_ANALOG_DIGPROG.&lt;/P&gt;&lt;P&gt;In this case, the added chip revisions (1.3, 1.4 and 1.5) are not used when rev 1.2 chip is used.&lt;/P&gt;&lt;P&gt;So I felt the patch is not necessary for rev 1.2 chip.&lt;/P&gt;&lt;P&gt;Is this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 05:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-i-MX6SDL-EB804/m-p/363318#M51343</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-08-18T05:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: Question about i.MX6SDL EB804.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-i-MX6SDL-EB804/m-p/363319#M51344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes for i.MX6SDL latest revision 1.2,&lt;/P&gt;&lt;P&gt;so patches for other (1.3, 1.5) are not needed.&lt;/P&gt;&lt;P&gt;Please note that Linux BSP is unified for all i.MX6 processors&lt;/P&gt;&lt;P&gt;so this patch is suggested to apply for providing universal solution&lt;/P&gt;&lt;P&gt;for all i.MX6 processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 05:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-i-MX6SDL-EB804/m-p/363319#M51344</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-18T05:45:56Z</dc:date>
    </item>
  </channel>
</rss>