<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Segmentation fault on camera module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168817#M5125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jimmy for Your answer,&lt;/P&gt;&lt;P&gt;But test for camera is write for EVK and I want to port it for LOCO board. So I've allredy did modifs on LOCO.c (QSB) to have my camera up but i have had the error You've seen in the first mesg. I will do somme work to try to adapt the camera tests for the QSB_LOCO.&lt;/P&gt;&lt;P&gt;Thanks again. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2012 21:45:25 GMT</pubDate>
    <dc:creator>luchurd</dc:creator>
    <dc:date>2012-11-12T21:45:25Z</dc:date>
    <item>
      <title>Segmentation fault on camera module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168815#M5123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;I have installed mt9v022 camera module on the IMX-53 QSB-LOCO and after modprobe I have this:&lt;/P&gt;&lt;P&gt;Unable to handle kernel paging request at virtual address 4e454796&lt;/P&gt;&lt;P&gt;pgd = df720000&lt;/P&gt;&lt;P&gt;[4e454796] *pgd=00000000&lt;/P&gt;&lt;P&gt;Internal error: Oops: 5 [#1] PREEMPT&lt;/P&gt;&lt;P&gt;last sysfs file: /sys/devices/virtual/input/input3/capabilities/sw&lt;/P&gt;&lt;P&gt;Modules linked in: mt9v022(+)&lt;/P&gt;&lt;P&gt;CPU: 0&amp;nbsp;&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (2.6.35.3-1129-g691c08a #25)&lt;/P&gt;&lt;P&gt;PC is at dev_get_drvdata+0x10/0x20&lt;/P&gt;&lt;P&gt;LR is at mt9v022_probe+0x12c/0x46c [mt9v022]&lt;/P&gt;&lt;P&gt;pc : [&amp;lt;8024000c&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;7f000fa0&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; psr: 20000013&lt;/P&gt;&lt;P&gt;sp : df72fe70&amp;nbsp; ip : 0000ffff&amp;nbsp; fp : 0000002e&lt;/P&gt;&lt;P&gt;r10: df702580&amp;nbsp; r9 : df72e000&amp;nbsp; r8 : 00000001&lt;/P&gt;&lt;P&gt;r7 : df144220&amp;nbsp; r6 : df702580&amp;nbsp; r5 : 80865fc8&amp;nbsp; r4 : df144200&lt;/P&gt;&lt;P&gt;r3 : 4e454756&amp;nbsp; r2 : 00000048&amp;nbsp; r1 : 00000001&amp;nbsp; r0 : 807b01a4&lt;/P&gt;&lt;P&gt;Flags: nzCv&amp;nbsp; IRQs on&amp;nbsp; FIQs on&amp;nbsp; Mode SVC_32&amp;nbsp; ISA ARM&amp;nbsp; Segment user&lt;/P&gt;&lt;P&gt;Control: 10c5387d&amp;nbsp; Table: cf720019&amp;nbsp; DAC: 00000015&lt;/P&gt;&lt;P&gt;Process insmod (pid: 2321, stack limit = 0xdf72e2e8)&lt;/P&gt;&lt;P&gt;Stack: (0xdf72fe70 to 0xdf730000)&lt;/P&gt;&lt;P&gt;fe60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; df144200 7f0013d8 00000000 df144220&lt;/P&gt;&lt;P&gt;fe80: 7f0013d8 df144200 7f000e74 df144204 df72e000 00004000 00000000 802d222c&lt;/P&gt;&lt;P&gt;fea0: df144220 df144254 7f001838 7f001838 80034104 80240418 df144220 df144254&lt;/P&gt;&lt;P&gt;fec0: 7f001838 00000000 80034104 80240534 7f001838 df72fee0 802404d4 8023fc28&lt;/P&gt;&lt;P&gt;fee0: df031838 df082570 7f001838 7f001838 df6d6120 8088f560 00000000 8023f564&lt;/P&gt;&lt;P&gt;ff00: 7f0017ce 7f0017ce 00000000 7f001838 00000000 7f001810 8088f560 80034104&lt;/P&gt;&lt;P&gt;ff20: 00004000 80240824 8088f53c 00000000 7f001810 8088f560 80034104 802d2f68&lt;/P&gt;&lt;P&gt;ff40: 7f004000 00000000 00000000 00003a49 80034104 80033380 7f004000 00000000&lt;/P&gt;&lt;P&gt;ff60: 00000001 00000000 7f001970 00000000 00012008 80034104 df72e000 00004000&lt;/P&gt;&lt;P&gt;ff80: 00000000 8008e788 00012018 00003a49 00012008 00000002 7ee42ec9 00012018&lt;/P&gt;&lt;P&gt;ffa0: 00000080 80033f80 00000002 7ee42ec9 00012018 00003a49 00012008 0000002d&lt;/P&gt;&lt;P&gt;ffc0: 00000002 7ee42ec9 00012018 00000080 00000003 00000000 00004000 00000000&lt;/P&gt;&lt;P&gt;ffe0: 00012008 7ee42c5c 0000892c 2ab94fc4 60000010 00012018 76dfdabf 8db85ff6&lt;/P&gt;&lt;P&gt;[&amp;lt;8024000c&amp;gt;] (dev_get_drvdata+0x10/0x20) from [&amp;lt;7f000fa0&amp;gt;] (mt9v022_probe+0x12c/0x46c [mt9v022])&lt;/P&gt;&lt;P&gt;[&amp;lt;7f000fa0&amp;gt;] (mt9v022_probe+0x12c/0x46c [mt9v022]) from [&amp;lt;802d222c&amp;gt;] (i2c_device_probe+0xa4/0xd8)&lt;/P&gt;&lt;P&gt;[&amp;lt;802d222c&amp;gt;] (i2c_device_probe+0xa4/0xd8) from [&amp;lt;80240418&amp;gt;] (driver_probe_device+0xc8/0x184)&lt;/P&gt;&lt;P&gt;[&amp;lt;80240418&amp;gt;] (driver_probe_device+0xc8/0x184) from [&amp;lt;80240534&amp;gt;] (__driver_attach+0x60/0x84)&lt;/P&gt;&lt;P&gt;[&amp;lt;80240534&amp;gt;] (__driver_attach+0x60/0x84) from [&amp;lt;8023fc28&amp;gt;] (bus_for_each_dev+0x48/0x84)&lt;/P&gt;&lt;P&gt;[&amp;lt;8023fc28&amp;gt;] (bus_for_each_dev+0x48/0x84) from [&amp;lt;8023f564&amp;gt;] (bus_add_driver+0x98/0x214)&lt;/P&gt;&lt;P&gt;[&amp;lt;8023f564&amp;gt;] (bus_add_driver+0x98/0x214) from [&amp;lt;80240824&amp;gt;] (driver_register+0xac/0x13c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80240824&amp;gt;] (driver_register+0xac/0x13c) from [&amp;lt;802d2f68&amp;gt;] (i2c_register_driver+0x40/0x8c)&lt;/P&gt;&lt;P&gt;[&amp;lt;802d2f68&amp;gt;] (i2c_register_driver+0x40/0x8c) from [&amp;lt;80033380&amp;gt;] (do_one_initcall+0x58/0x1b0)&lt;/P&gt;&lt;P&gt;[&amp;lt;80033380&amp;gt;] (do_one_initcall+0x58/0x1b0) from [&amp;lt;8008e788&amp;gt;] (sys_init_module+0x90/0x1ac)&lt;/P&gt;&lt;P&gt;[&amp;lt;8008e788&amp;gt;] (sys_init_module+0x90/0x1ac) from [&amp;lt;80033f80&amp;gt;] (ret_fast_syscall+0x0/0x30)&lt;/P&gt;&lt;P&gt;Code: e3500000 0a000003 e5903004 e3530000 (15930040) &lt;/P&gt;&lt;P&gt;---[ end trace 878551c919f71e5a ]---&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help on this?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Nov 2012 21:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168815#M5123</guid>
      <dc:creator>luchurd</dc:creator>
      <dc:date>2012-11-08T21:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: Segmentation fault on camera module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168816#M5124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to read the CSI document to make it work.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="301558" data-objecttype="1" href="https://community.nxp.com/thread/301558"&gt;https://community.freescale.com/thread/301558&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 02:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168816#M5124</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-11-12T02:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: Segmentation fault on camera module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168817#M5125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jimmy for Your answer,&lt;/P&gt;&lt;P&gt;But test for camera is write for EVK and I want to port it for LOCO board. So I've allredy did modifs on LOCO.c (QSB) to have my camera up but i have had the error You've seen in the first mesg. I will do somme work to try to adapt the camera tests for the QSB_LOCO.&lt;/P&gt;&lt;P&gt;Thanks again. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 21:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-on-camera-module/m-p/168817#M5125</guid>
      <dc:creator>luchurd</dc:creator>
      <dc:date>2012-11-12T21:45:25Z</dc:date>
    </item>
  </channel>
</rss>