<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 WATCH DOG PINS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-WATCH-DOG-PINS/m-p/362498#M51123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After going through the watchdog signal description given in iMXDQRM(page 5744,5755) I did understand that there are two signals getting generated in case of watchdog event.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. WDOG_B&lt;/P&gt;&lt;P&gt;2. WDOG_RESET_B_DEB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me understand how the watchdog function is implemented with respect to the above mentioned signals in sabre-sd board so that I can practically understand the significance of each of those signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, what are the input and output pins of WatchDog unit exposed to user?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my application, there are 2 processors. I want the WDOG-OUT of each processor to be monitored by the other processor. In this scenario, let me know where I should connect(which pin) the WDOG-OUT(timeout signal) of one processor as input to another processor in order to generate a global reset for the system. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know in case you need any clarification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 Aug 2014 08:02:39 GMT</pubDate>
    <dc:creator>vigneshvasudeva</dc:creator>
    <dc:date>2014-08-17T08:02:39Z</dc:date>
    <item>
      <title>i.MX6 WATCH DOG PINS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-WATCH-DOG-PINS/m-p/362498#M51123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After going through the watchdog signal description given in iMXDQRM(page 5744,5755) I did understand that there are two signals getting generated in case of watchdog event.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. WDOG_B&lt;/P&gt;&lt;P&gt;2. WDOG_RESET_B_DEB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me understand how the watchdog function is implemented with respect to the above mentioned signals in sabre-sd board so that I can practically understand the significance of each of those signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, what are the input and output pins of WatchDog unit exposed to user?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my application, there are 2 processors. I want the WDOG-OUT of each processor to be monitored by the other processor. In this scenario, let me know where I should connect(which pin) the WDOG-OUT(timeout signal) of one processor as input to another processor in order to generate a global reset for the system. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know in case you need any clarification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Aug 2014 08:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-WATCH-DOG-PINS/m-p/362498#M51123</guid>
      <dc:creator>vigneshvasudeva</dc:creator>
      <dc:date>2014-08-17T08:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 WATCH DOG PINS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-WATCH-DOG-PINS/m-p/362499#M51124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vignesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WDOG_RESET_B_DEB is internal processor signal,&lt;/P&gt;&lt;P&gt;WDOG_B is external - it can be used for board reset, example&lt;/P&gt;&lt;P&gt;can be found on Sabre SD schematic SPF-27392 p.21&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Aug 2014 12:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-WATCH-DOG-PINS/m-p/362499#M51124</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-17T12:51:01Z</dc:date>
    </item>
  </channel>
</rss>