<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6/SABRE-AI base board bluetooth issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-base-board-bluetooth-issue/m-p/361913#M50991</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to develop Bluetooth software on iMX6, my device is iMX6QAICPU board and SABRE-AI base board.&lt;/P&gt;&lt;P&gt;I already connected CSR 8311 BT chip to BT Module Connector (J32) of SABRE-AI base board.&lt;/P&gt;&lt;P&gt;As I can see from system there is 3 UART port:&lt;/P&gt;&lt;P&gt;ttymxc1, &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ttymxc2 and &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ttymxc3 (debug port)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;We test ttymxc1 and ttymxc2 but both are fail to read/write.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Which UART device should be used for this BT module connector (J32) ? or should I modify anything from BSP first?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Thank you for help...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Tayler&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 01:45:17 GMT</pubDate>
    <dc:creator>taylerko</dc:creator>
    <dc:date>2014-10-02T01:45:17Z</dc:date>
    <item>
      <title>iMX6/SABRE-AI base board bluetooth issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-base-board-bluetooth-issue/m-p/361913#M50991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to develop Bluetooth software on iMX6, my device is iMX6QAICPU board and SABRE-AI base board.&lt;/P&gt;&lt;P&gt;I already connected CSR 8311 BT chip to BT Module Connector (J32) of SABRE-AI base board.&lt;/P&gt;&lt;P&gt;As I can see from system there is 3 UART port:&lt;/P&gt;&lt;P&gt;ttymxc1, &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ttymxc2 and &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ttymxc3 (debug port)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;We test ttymxc1 and ttymxc2 but both are fail to read/write.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Which UART device should be used for this BT module connector (J32) ? or should I modify anything from BSP first?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Thank you for help...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Tayler&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 01:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-base-board-bluetooth-issue/m-p/361913#M50991</guid>
      <dc:creator>taylerko</dc:creator>
      <dc:date>2014-10-02T01:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6/SABRE-AI base board bluetooth issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-base-board-bluetooth-issue/m-p/361914#M50992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tailer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is &lt;SPAN style="font-size: 10pt;"&gt;ttymxc2 (UART3) you can check &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6_SABRE_AI_DESIGNFILES&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Design files&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;p.20 SCH-27142&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;also please check below for supported BT chips&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95006"&gt;142-00207-517_iMX6X_SX-SDCAN_BT.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94235"&gt;How to enable BT on board imx6q_sabresd RevC.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX_6Dual6Quad_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;Chapter 41Bluetooth Driver &lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale BSP does not support/provide CSR BT driver one &lt;/P&gt;&lt;P&gt;needs to apply for help to vendor of these chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 10:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-base-board-bluetooth-issue/m-p/361914#M50992</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-02T10:26:03Z</dc:date>
    </item>
  </channel>
</rss>