<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6: TW8836_TVIN(BT656) ===&amp;gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360514#M50664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Friends,&lt;/P&gt;&lt;P&gt;My V4L2 TVin driver is working. Its all about sensor configuration...^^&lt;/P&gt;&lt;P&gt;FAE gave me another set of tw8836 codec configuration and it just worked and now we can see video input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fortunately I myself answering my question :smileyhappy: (lol)&lt;/P&gt;&lt;P&gt;My Suggestions, Just follow tvin reference driver adv7180 given by Freescale and configure your sensor/videocodec chip with right values.&lt;/P&gt;&lt;P&gt;and run mxc_v4l2_tvin -ow 720 -oh 480 -ol 10 -ot 20. If it at all there is a problem, you can assume that its problem with HW or sensor configuration.&lt;/P&gt;&lt;P&gt;Make sure pclk(27MHz) and your input must be standard UYUV / YCbCr 4:2:2 NTSC / PAL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51058iE5D9743B932AEF0E/image-size/large?v=v2&amp;amp;px=999" title="20150402_153117.jpg" alt="20150402_153117.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rajucm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Apr 2015 08:17:57 GMT</pubDate>
    <dc:creator>rajucm</dc:creator>
    <dc:date>2015-04-02T08:17:57Z</dc:date>
    <item>
      <title>I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360510#M50660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;We are developing TVIN V4L2 Slave driver for TW8836 (Video codec Chip from I).&lt;/P&gt;&lt;P&gt;This VCODEC chip can output BT656 standard YCbCr (8bit) NTSC/PAL video standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my schematic,&lt;/P&gt;&lt;P&gt;TW8836(VCODEC) ===connected===&amp;gt;IMx6q's CSI0 (CSI0_DAT12 : CSI0_DAT19).&lt;/P&gt;&lt;P&gt;It also has HSYNC &amp;amp; VSYNC Lines for video synchronization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have followed, ADV7180 as a example driver and initialized TW8836 with vendor recommended values using I2C.&lt;/P&gt;&lt;P&gt;I used following IOCTL callback to configure TW8836&lt;/P&gt;&lt;P&gt;=================================================================================================&lt;/P&gt;&lt;P&gt;static int ioctl_dev_init(struct v4l2_int_device *s)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int ret;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; tw8836_data.on = true;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pr_debug("In tw8836:ioctl_dev_init\n");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ret = tw8836_chip_init();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // &amp;lt;--- Configure TW8836 to output BT656 standard video&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configurations were given by TW8836 vendor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return ret;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We further check that, I2C read/Writes are perfect and sensor configured for given values.&lt;/P&gt;&lt;P&gt;Also we measured, Pix-clock using scope i.e 27MHz (cool.. I believe it is as per standard).&lt;/P&gt;&lt;P&gt;====================================================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, I tried using mxc_v4l2_tvin application as recommended as follows...&lt;/P&gt;&lt;P&gt;root@sabresd_6dq:/ # mxc_v4l2_tvin -ow 720 -oh 525 -ol 10 -ot 20 -f YUV422&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mxc_v4l2_tvin -ow 720 -oh 480 -ol 20&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TV decoder chip is tw8836_decoder&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; driver=mxc_vout, card=DISP3 FG, bus=, version=0x00000000, capabilities=0x04000002&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt RGB565: fourcc = 0x50424752&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt BGR24: fourcc = 0x33524742&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt RGB24: fourcc = 0x33424752&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt RGB32: fourcc = 0x34424752&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt BGR32: fourcc = 0x34524742&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt NV12: fourcc = 0x3231564e&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt UYVY: fourcc = 0x59565955&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YUYV: fourcc = 0x56595559&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YUV422 planar: fourcc = 0x50323234&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YUV444: fourcc = 0x34343459&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YUV420: fourcc = 0x32315559&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YVU420: fourcc = 0x32315659&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt TILED NV12P: fourcc = 0x50564e54&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt TILED NV12F: fourcc = 0x46564e54&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fmt YUV444 planar: fourcc = 0x50343434&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start time = 86476 s, 582752 us&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now what we can see is, a window is displayed with noise (may be white noise). I have updated screen snap shot (pleas check).&lt;/P&gt;&lt;P&gt;Can any one give me some hint. What could be gone wrong???&amp;nbsp;&amp;nbsp; Please lemme know if more info needed...&lt;/P&gt;&lt;P class="menuItems"&gt;&lt;A class="menuItem_jiveImageItem button"&gt;javascript:;&lt;/A&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47983i097DF7DCE718CEB1/image-size/large?v=v2&amp;amp;px=999" title="20150328_1538.jpg" alt="20150328_1538.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rajucm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Mar 2015 07:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360510#M50660</guid>
      <dc:creator>rajucm</dc:creator>
      <dc:date>2015-03-28T07:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360511#M50661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;May I get some help on this... please give me some direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Raju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 03:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360511#M50661</guid>
      <dc:creator>rajucm</dc:creator>
      <dc:date>2015-03-30T03:32:47Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360512#M50662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;Some info,&lt;/P&gt;&lt;P&gt;as explained in &lt;A href="https://community.nxp.com/docs/DOC-93633"&gt;De-interlace Capture Device&lt;/A&gt; I have applied&lt;A _jive_internal="true" class="j-attachment-icon" data-content-finding="Community" href="https://community.nxp.com/servlet/JiveServlet/download/93633-3-252351/add-csi-deinterlace-capture.patch.zip"&gt; &lt;/A&gt;&lt;A _jive_internal="true" data-content-finding="Community" href="https://community.nxp.com/servlet/JiveServlet/download/93633-3-252351/add-csi-deinterlace-capture.patch.zip"&gt;add-csi-deinterlace-capture.patch.zip&lt;/A&gt; patch.&lt;/P&gt;&lt;P&gt;From logs evry thing looks ok. Isee propes Que &amp;amp; Dequeue Buffer.&lt;/P&gt;&lt;P&gt;But still I see white noise as uploaded in above pic. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please gimme some pointer.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@sabresd_6dq:/ # mxc_v4l2_tvin -ow 720 -oh 480 -ol 10 -ot 20&lt;/P&gt;&lt;P&gt;mxc_v4l2_tvin -ow 720 -oh 480 -ol 10 -ot 20&lt;/P&gt;&lt;P&gt;TV decoder chip is ov5640_camera&lt;/P&gt;&lt;P&gt;driver=mxc_vout, card=DISP3 FG, bus=, version=0x00000000, capabilities=0x04000002&lt;/P&gt;&lt;P&gt;fmt RGB565: fourcc = 0x50424752&lt;/P&gt;&lt;P&gt;fmt BGR24: fourcc = 0x33524742&lt;/P&gt;&lt;P&gt;fmt RGB24: fourcc = 0x33424752&lt;/P&gt;&lt;P&gt;fmt RGB32: fourcc = 0x34424752&lt;/P&gt;&lt;P&gt;fmt BGR32: fourcc = 0x34524742&lt;/P&gt;&lt;P&gt;fmt NV12: fourcc = 0x3231564e&lt;/P&gt;&lt;P&gt;fmt UYVY: fourcc = 0x59565955&lt;/P&gt;&lt;P&gt;fmt YUYV: fourcc = 0x56595559&lt;/P&gt;&lt;P&gt;fmt YUV422 planar: fourcc = 0x50323234&lt;/P&gt;&lt;P&gt;fmt YUV444: fourcc = 0x34343459&lt;/P&gt;&lt;P&gt;fmt YUV420: fourcc = 0x32315559&lt;/P&gt;&lt;P&gt;fmt YVU420: fourcc = 0x32315659&lt;/P&gt;&lt;P&gt;fmt TILED NV12P: fourcc = 0x50564e54&lt;/P&gt;&lt;P&gt;fmt TILED NV12F: fourcc = 0x46564e54&lt;/P&gt;&lt;P&gt;fmt YUV444 planar: fourcc = 0x50343434&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=========================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MVC: mxc_v4l_open&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1606&amp;nbsp;&amp;nbsp;&amp;nbsp; device name is Mxc Camera&lt;/P&gt;&lt;P&gt;ioctl_g_ifparm 276 TW8836: tw8836_p ioctl_g_ifparm&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 332 TW8836: V4L2_BUF_TYPE_VIDEO_CAPTURE Returning size of 720x525&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1705 End of mxc_v4l_open: v2f pix widthxheight 720 x 480&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1708 End of mxc_v4l_open: crop_bounds widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1711 End of mxc_v4l_open: crop_defrect widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1714 End of mxc_v4l_open: crop_current widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l_open 1718 On Open: Input to ipu size is 720 x 525&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: CSI_SENS_CONF = 0x00000A02&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: CSI_ACT_FRM_SIZE = 0x020C02CF&lt;/P&gt;&lt;P&gt;In tw8836:ioctl_s_power 1&lt;/P&gt;&lt;P&gt;In tw8836:ioctl_init&lt;/P&gt;&lt;P&gt;ioctl_dev_init 224 TW8836: In tw8836:ioctl_dev_init&lt;/P&gt;&lt;P&gt;tw8836_chip_init 196 TW8836: ==&amp;gt; called, Initialize CVBS IN to PLAIN BT656 OUT&lt;/P&gt;&lt;P&gt;tw8836_write_reg 142 TW8836: PAGE Reg value changed to ox0&lt;/P&gt;&lt;P&gt;tw8836_write_reg 142 TW8836: PAGE Reg value changed to ox1&lt;/P&gt;&lt;P&gt;tw8836_write_reg 142 TW8836: PAGE Reg value changed to ox2&lt;/P&gt;&lt;P&gt;tw8836_write_reg 142 TW8836: PAGE Reg value changed to ox6&lt;/P&gt;&lt;P&gt;tw8836 0-0045: INIT DONE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80685600&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1953&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYCAP&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c02c5651&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0045627&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2354&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_S_INPUT 1&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 40085618&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2298&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_S_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_std 1456 In mxc_v4l2_s_std b000&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_std 1464&amp;nbsp;&amp;nbsp;&amp;nbsp; Setting standard to NTSC b000&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c02c563a&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2140&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_CROPCAP&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0cc5616&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2266&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_S_PARM&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1320 In mxc_v4l2_s_param&lt;/P&gt;&lt;P&gt;In tw8836:ioctl_g_parm&lt;/P&gt;&lt;P&gt;ioctl_g_parm 370 TW8836:&amp;nbsp;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1348&amp;nbsp;&amp;nbsp;&amp;nbsp; Current capabilities are 0&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1351&amp;nbsp;&amp;nbsp;&amp;nbsp; Current capturemode is 0&amp;nbsp; change to 0&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1353&amp;nbsp;&amp;nbsp;&amp;nbsp; Current framerate is 30&amp;nbsp; change to 0&lt;/P&gt;&lt;P&gt;In tw8836:ioctl_s_parm&lt;/P&gt;&lt;P&gt;ioctl_g_ifparm 276 TW8836: tw8836_p ioctl_g_ifparm&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1382&amp;nbsp;&amp;nbsp;&amp;nbsp; clock_curr=mclk=0&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 332 TW8836: V4L2_BUF_TYPE_VIDEO_CAPTURE Returning size of 720x525&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_param 1407&amp;nbsp;&amp;nbsp;&amp;nbsp; g_fmt_cap returns widthxheight of input as 720 x 525&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: CSI_SENS_CONF = 0x00008A32&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: CSI_ACT_FRM_SIZE = 0x01DF02CF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0cc5605&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1980&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_S_FMT&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 817 In MVC: mxc_v4l2_s_fmt&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 821&amp;nbsp;&amp;nbsp;&amp;nbsp; type=V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 959 End of mxc_v4l2_s_fmt: v2f pix widthxheight 720 x 480&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 962 End of mxc_v4l2_s_fmt: crop_bounds widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 965 End of mxc_v4l2_s_fmt: crop_defrect widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l2_s_fmt 968 End of mxc_v4l2_s_fmt: crop_current widthxheight 720 x 480&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0cc5604&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1970&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_FMT&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 769 In MVC: mxc_v4l2_g_fmt type=1&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 773&amp;nbsp;&amp;nbsp;&amp;nbsp; type is V4L2_BUF_TYPE_VIDEO_CAPTURE&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 787 End of mxc_v4l2_g_fmt: v2f pix widthxheight 720 x 480&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 790 End of mxc_v4l2_g_fmt: crop_bounds widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 793 End of mxc_v4l2_g_fmt: crop_defrect widthxheight 720 x 525&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_fmt 796 End of mxc_v4l2_g_fmt: crop_current widthxheight 720 x 480&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0145608&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1990&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_REQBUFS&lt;/P&gt;&lt;P&gt;mxc_streamoff 497 In MVC:mxc_streamoff&lt;/P&gt;&lt;P&gt;mxc_free_frame_buf 241 MVC: In mxc_free_frame_buf&lt;/P&gt;&lt;P&gt;mxc_allocate_frame_buf 268 In MVC:mxc_allocate_frame_buf - size=691200&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445609&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2019&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;/P&gt;&lt;P&gt;mxc_v4l2_buffer_status 328 In MVC:mxc_v4l2_buffer_status&lt;/P&gt;&lt;P&gt;mxc_mmap 2478 In MVC:mxc_mmap&lt;/P&gt;&lt;P&gt;mxc_mmap 2480&amp;nbsp;&amp;nbsp;&amp;nbsp; pgoff=0x21a00, start=0x40738000, end=0x407e1000&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445609&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2019&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;/P&gt;&lt;P&gt;mxc_v4l2_buffer_status 328 In MVC:mxc_v4l2_buffer_status&lt;/P&gt;&lt;P&gt;mxc_mmap 2478 In MVC:mxc_mmap&lt;/P&gt;&lt;P&gt;mxc_mmap 2480&amp;nbsp;&amp;nbsp;&amp;nbsp; pgoff=0x21b00, start=0x40831000, end=0x408da000&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445609&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2019&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QUERYBUF&lt;/P&gt;&lt;P&gt;mxc_v4l2_buffer_status 328 In MVC:mxc_v4l2_buffer_status&lt;/P&gt;&lt;P&gt;mxc_mmap 2478 In MVC:mxc_mmap&lt;/P&gt;&lt;P&gt;mxc_mmap 2480&amp;nbsp;&amp;nbsp;&amp;nbsp; pgoff=0x1e000, start=0x409a9000, end=0x40a52000&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 40045612&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2103&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_STREAMON&lt;/P&gt;&lt;P&gt;mxc_streamon 409 In MVC:mxc_streamon&lt;/P&gt;&lt;P&gt;mxc_streamon 445 Debug pointer&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;camera_callback 2578 In MVC:camera_callback&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c044560f&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2052&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_QBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl 80085617&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2286&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_G_STD&lt;/P&gt;&lt;P&gt;mxc_v4l2_g_std 1502 In mxc_v4l2_g_std&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 326 TW8836:&lt;/P&gt;&lt;P&gt;ioctl_g_fmt_cap 337 TW8836: V4L2_BUF_TYPE_PRIVATE&lt;/P&gt;&lt;P&gt;mxc_v4l_ioctl 2458 In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 1940 In MVC: mxc_v4l_do_ioctl c0445611&lt;/P&gt;&lt;P&gt;mxc_v4l_do_ioctl 2087&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_DQBUF&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1542 In MVC:mxc_v4l_dqueue&lt;/P&gt;&lt;P&gt;mxc_v4l_dqueue 1552 ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received&lt;/P&gt;&lt;P&gt;mxc_v4l_close 1761 In MVC:mxc_v4l_close&lt;/P&gt;&lt;P&gt;mxc_streamoff 497 In MVC:mxc_streamoff&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: CSI stop timeout - 5 * 10ms&lt;/P&gt;&lt;P&gt;mxc_free_frames 306 In MVC:mxc_free_frames&lt;/P&gt;&lt;P&gt;In tw8836:ioctl_s_power 0&lt;/P&gt;&lt;P&gt;mxc_v4l_close 1793 mxc_v4l_close: release resource&lt;/P&gt;&lt;P&gt;mxc_free_frame_buf 241 MVC: In mxc_free_frame_buf&lt;/P&gt;&lt;P&gt;mxc_free_frames 306 In MVC:mxc_free_frames&lt;/P&gt;&lt;P&gt;init: untracked pid 3069 exited&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 06:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360512#M50662</guid>
      <dc:creator>rajucm</dc:creator>
      <dc:date>2015-03-30T06:39:55Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360513#M50663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think it look like I am getting data from sensor....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_v4l2_tvin directly dump the data to FB0, &lt;/P&gt;&lt;P&gt;Can any one tell me how to store this data in yuv file. So that at least I can play using YUV player and test.&lt;/P&gt;&lt;P&gt;any help would be appreciated...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Raju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 13:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360513#M50663</guid>
      <dc:creator>rajucm</dc:creator>
      <dc:date>2015-03-30T13:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360514#M50664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Friends,&lt;/P&gt;&lt;P&gt;My V4L2 TVin driver is working. Its all about sensor configuration...^^&lt;/P&gt;&lt;P&gt;FAE gave me another set of tw8836 codec configuration and it just worked and now we can see video input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fortunately I myself answering my question :smileyhappy: (lol)&lt;/P&gt;&lt;P&gt;My Suggestions, Just follow tvin reference driver adv7180 given by Freescale and configure your sensor/videocodec chip with right values.&lt;/P&gt;&lt;P&gt;and run mxc_v4l2_tvin -ow 720 -oh 480 -ol 10 -ot 20. If it at all there is a problem, you can assume that its problem with HW or sensor configuration.&lt;/P&gt;&lt;P&gt;Make sure pclk(27MHz) and your input must be standard UYUV / YCbCr 4:2:2 NTSC / PAL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51058iE5D9743B932AEF0E/image-size/large?v=v2&amp;amp;px=999" title="20150402_153117.jpg" alt="20150402_153117.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rajucm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 08:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360514#M50664</guid>
      <dc:creator>rajucm</dc:creator>
      <dc:date>2015-04-02T08:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360515#M50665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rajucm"&gt;rajucm&lt;/A&gt;​, can you share your vendor provided &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;tw8836_chip_init()&lt;/SPAN&gt; code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 19:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360515#M50665</guid>
      <dc:creator>curtl</dc:creator>
      <dc:date>2015-12-28T19:05:45Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360516#M50666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can get init code of tw**** form vendor. My tw9900 is working now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 00:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360516#M50666</guid>
      <dc:creator>echozeng</dc:creator>
      <dc:date>2016-06-22T00:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360517#M50667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raju CM,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We also using TW8836 chip for other application and glad to hear success case!!&lt;/P&gt;&lt;P&gt;As you say::&lt;/P&gt;&lt;P&gt;"Make sure pclk(27MHz) and your input must be standard UYUV / YCbCr 4:2:2 NTSC / PAL."&lt;/P&gt;&lt;P&gt;But i.mx6 only support&amp;nbsp; YUV422 (YUYV) and YUV422 (UYVY) input format, not include UYUV...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do we need to do format converter or not ? Or what kind of pixelformat you use ? Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;David Wu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 01:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360517#M50667</guid>
      <dc:creator>david5icp</dc:creator>
      <dc:date>2016-07-05T01:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360518#M50668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please provide your driver for the TW9900? I'm also planning to use that video-adc; would be nice to have some code to start with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 06:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360518#M50668</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2016-07-05T06:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6: TW8836_TVIN(BT656) ===&gt; CSI0 (8-Bit / CSI0_DAT12 : CSI0_DAT19)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360519#M50669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;please email to&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:zengzh@139.com"&gt;zengzh@139.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 07:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-TW8836-TVIN-BT656-gt-CSI0-8-Bit-CSI0-DAT12-CSI0-DAT19/m-p/360519#M50669</guid>
      <dc:creator>echozeng</dc:creator>
      <dc:date>2016-07-06T07:16:41Z</dc:date>
    </item>
  </channel>
</rss>