<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MX6SL_EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359845#M50543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, good day eveybody, i config file board-mx6sl_evk.c, i refer file config guide for board mx50. i see it's configed:&lt;/P&gt;&lt;P&gt;+static iomux_v3_cfg_t mx50_t15dds15_pads_disabled[] = {&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D0__GPIO_2_0,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D1__GPIO_2_1,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D2__GPIO_2_2,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D3__GPIO_2_3,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D4__GPIO_2_4,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D5__GPIO_2_5,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D6__GPIO_2_6,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D7__GPIO_2_7,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_WR__GPIO_2_16,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RS__GPIO_2_17,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RD__GPIO_2_19,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RESET__GPIO_2_20,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_CS__GPIO_2_21,&lt;/P&gt;&lt;P&gt;+};&lt;/P&gt;&lt;P&gt;what is DISP? in imx6sl not have DISP., what is function?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Oct 2014 04:21:16 GMT</pubDate>
    <dc:creator>phamhuynh</dc:creator>
    <dc:date>2014-10-01T04:21:16Z</dc:date>
    <item>
      <title>MX6SL_EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359845#M50543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, good day eveybody, i config file board-mx6sl_evk.c, i refer file config guide for board mx50. i see it's configed:&lt;/P&gt;&lt;P&gt;+static iomux_v3_cfg_t mx50_t15dds15_pads_disabled[] = {&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D0__GPIO_2_0,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D1__GPIO_2_1,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D2__GPIO_2_2,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D3__GPIO_2_3,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D4__GPIO_2_4,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D5__GPIO_2_5,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D6__GPIO_2_6,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_D7__GPIO_2_7,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_WR__GPIO_2_16,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RS__GPIO_2_17,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RD__GPIO_2_19,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_RESET__GPIO_2_20,&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; MX50_PAD_DISP_CS__GPIO_2_21,&lt;/P&gt;&lt;P&gt;+};&lt;/P&gt;&lt;P&gt;what is DISP? in imx6sl not have DISP., what is function?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 04:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359845#M50543</guid>
      <dc:creator>phamhuynh</dc:creator>
      <dc:date>2014-10-01T04:21:16Z</dc:date>
    </item>
    <item>
      <title>Re: MX6SL_EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359846#M50544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IMX50 has eLCDIF similar to one of i.MX28 and i.MX6 SL.&lt;/P&gt;&lt;P&gt;In Table 4-1 (Pin Assignments Report) of the i.MX50 Reference&lt;/P&gt;&lt;P&gt;Manual corresponding signals / pins are named with prefix DISP,&lt;/P&gt;&lt;P&gt;but in Chapter 37 [Enhanced LCD Interface (eLCDIF)] the same signals&lt;/P&gt;&lt;P&gt;are used with prefix LCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 04:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359846#M50544</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-01T04:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: MX6SL_EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359847#M50545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, but so i config pin for i.MX6Sl, i don't need have DISP, don't you?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 07:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359847#M50545</guid>
      <dc:creator>phamhuynh</dc:creator>
      <dc:date>2014-10-01T07:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: MX6SL_EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359848#M50546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At least display / LCDIF pins of the i.MX6 SL should be configured properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 07:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6SL-EVK/m-p/359848#M50546</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-01T07:19:05Z</dc:date>
    </item>
  </channel>
</rss>