<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX28 Power and Crystal problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Power-and-Crystal-problem/m-p/359323#M50471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IMX28 VDDIO33 must be in range 3.0 - 3.6 V.&lt;/P&gt;&lt;P&gt;Please try to provide it - at least - as first step.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Aug 2014 00:42:31 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-08-15T00:42:31Z</dc:date>
    <item>
      <title>i.MX28 Power and Crystal problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Power-and-Crystal-problem/m-p/359322#M50470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm currently debbuging a custom board based on the imx28evk schematic using an i.MX287. I'm using u-boot 2014-07 on a SD Card, and everything work fine on the imx28evk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my custom board, u-boot is not working, but i'm able to print debug info from spl_boot.c. After that, nothing. The baudrate on the DUART is around 100000 bauds on my board instead of 115200 on the evk (with the same sd card).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reviewing my schematic, i've found that VDDIO33_EMI is connected to VDDIO_1V8 instead of VDDIO_3V3. Since this trace is under the imx28, I would like to confirm that my problems are related to this before making a new board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I probe the VDDIO_3V3 and VDDIO_1V8 rails, I measure a clean 3.3V and 1.8V. On the VDDIO33_EMI pin, I measure 1.8V. I can't find info in the datasheets about the difference between VDDIO33_x pins and VDDIO33_EMI pin. Are they link together internally?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VDD4P2 linreg seems to start, but fall to 0V after 1s. My board is powered only by a 5V reg and the LI-ON_BATTERY net is not connected to an external regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the EVK without the SD Card and I probe the crystal, I can see a clean 24MHz with a 500mVDC offset. When I boot my custom board (without the SD card), I see a flat 1VDC for about 2s, and then only 500mVDC. I'm using a C0603C180J5GACTU crystal (which seem very similar to the one on the evk: CS10-24.000MABJ-UT) with 18pf capacitors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you think that all thoses issues are related to the VDDIO33_EMI wrong connection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 15:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Power-and-Crystal-problem/m-p/359322#M50470</guid>
      <dc:creator>spicard</dc:creator>
      <dc:date>2014-08-14T15:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 Power and Crystal problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Power-and-Crystal-problem/m-p/359323#M50471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IMX28 VDDIO33 must be in range 3.0 - 3.6 V.&lt;/P&gt;&lt;P&gt;Please try to provide it - at least - as first step.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Aug 2014 00:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Power-and-Crystal-problem/m-p/359323#M50471</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-08-15T00:42:31Z</dc:date>
    </item>
  </channel>
</rss>