<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMPF0100F3AEP LiCell Pin Connection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100F3AEP-LiCell-Pin-Connection/m-p/359237#M50451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a design including i.Mx6 SoloLite Processor,with PMIC version "MMPF0100F3AEP" and without any Coin Cell, whether do we need to bypass with a 0.1uF to ground , or do we need to connect the pin to a valid voltage source ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Mar 2015 06:49:05 GMT</pubDate>
    <dc:creator>pankajrana</dc:creator>
    <dc:date>2015-03-28T06:49:05Z</dc:date>
    <item>
      <title>MMPF0100F3AEP LiCell Pin Connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100F3AEP-LiCell-Pin-Connection/m-p/359237#M50451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a design including i.Mx6 SoloLite Processor,with PMIC version "MMPF0100F3AEP" and without any Coin Cell, whether do we need to bypass with a 0.1uF to ground , or do we need to connect the pin to a valid voltage source ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Mar 2015 06:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100F3AEP-LiCell-Pin-Connection/m-p/359237#M50451</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2015-03-28T06:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100F3AEP LiCell Pin Connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100F3AEP-LiCell-Pin-Connection/m-p/359238#M50452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can just bypass the LICELL pin to ground through a 0.1uF capacitor and do nothing else.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Mar 2015 08:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100F3AEP-LiCell-Pin-Connection/m-p/359238#M50452</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-03-29T08:51:23Z</dc:date>
    </item>
  </channel>
</rss>