<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eMMC on U-Boot -- Card did not respond to voltage select! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-on-U-Boot-Card-did-not-respond-to-voltage-select/m-p/358704#M50303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my custom board based on SabreSD, I'm trying to access to eMMC on U-Boot. But I get the statement "Card did not respond to voltage select!".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Main differences to Sabre-SD:&lt;/P&gt;&lt;P&gt;- My boot device is SPI NOR flash. I downloaded the U-Boot to SPI NOR flash with MFGTool and it seems to be running without a problem.&lt;/P&gt;&lt;P&gt;- eMMC is located on uSDHC3 rather than uSDHC4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've modified the port configurations for uSDHC3 port. Below is the console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.04 (Feb 06 2015 - 17:58:09)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6SOLO rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 41 C, calibration data: 0x5844f469&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: i.MX6 on ...&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 512 MiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;&lt;P&gt;SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Found PFUZE100 deviceid=10,revid=11&lt;/P&gt;&lt;P&gt;SW3 = 1.35V...&lt;/P&gt;&lt;P&gt;SW2 = 3.3V...&lt;/P&gt;&lt;P&gt;SW4 = 1.2V...&lt;/P&gt;&lt;P&gt;VGEN4 = 2.5V...&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;/P&gt;&lt;P&gt;Warning: failed to set MAC address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normal Boot&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp; 2&amp;nbsp; 1&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; &lt;/P&gt;&lt;P&gt;=&amp;gt; mmc rescan&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc dev&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;mmc0(part 0) is current device&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc dev 2&lt;/P&gt;&lt;P&gt;CMD_SEND:0&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_NONE&lt;/P&gt;&lt;P&gt;CMD_SEND:8&lt;/P&gt;&lt;P&gt;ARG 0x000001AA&lt;/P&gt;&lt;P&gt;MMC_RSP_R1,5,6,7&amp;nbsp; 0x2F551248 &lt;/P&gt;&lt;P&gt;CMD_SEND:55&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_R1,5,6,7&amp;nbsp; 0x2F551248 &lt;/P&gt;&lt;P&gt;CMD_SEND:0&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_NONE&lt;/P&gt;&lt;P&gt;CMD_SEND:1&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_R3,4 0x00010000 &lt;/P&gt;&lt;P&gt;Card did not respond to voltage select!&lt;/P&gt;&lt;P&gt;mmc2(part 0) is current device&lt;/P&gt;&lt;P&gt;=&amp;gt; &amp;lt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had also defined CONFIG_MMC_TRACE to get more information about what was going on.&lt;/P&gt;&lt;P&gt;eMMC memory seems to be returning some responses, though I could not find what to make of them.&lt;/P&gt;&lt;P&gt;Does that mean there is no hardware issue since it returns these responses?&lt;/P&gt;&lt;P&gt;If so, what could be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Feb 2015 07:42:10 GMT</pubDate>
    <dc:creator>durmus</dc:creator>
    <dc:date>2015-02-09T07:42:10Z</dc:date>
    <item>
      <title>eMMC on U-Boot -- Card did not respond to voltage select!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-on-U-Boot-Card-did-not-respond-to-voltage-select/m-p/358704#M50303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my custom board based on SabreSD, I'm trying to access to eMMC on U-Boot. But I get the statement "Card did not respond to voltage select!".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Main differences to Sabre-SD:&lt;/P&gt;&lt;P&gt;- My boot device is SPI NOR flash. I downloaded the U-Boot to SPI NOR flash with MFGTool and it seems to be running without a problem.&lt;/P&gt;&lt;P&gt;- eMMC is located on uSDHC3 rather than uSDHC4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've modified the port configurations for uSDHC3 port. Below is the console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.04 (Feb 06 2015 - 17:58:09)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6SOLO rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 41 C, calibration data: 0x5844f469&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: i.MX6 on ...&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 512 MiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;&lt;P&gt;SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Found PFUZE100 deviceid=10,revid=11&lt;/P&gt;&lt;P&gt;SW3 = 1.35V...&lt;/P&gt;&lt;P&gt;SW2 = 3.3V...&lt;/P&gt;&lt;P&gt;SW4 = 1.2V...&lt;/P&gt;&lt;P&gt;VGEN4 = 2.5V...&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;/P&gt;&lt;P&gt;Warning: failed to set MAC address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normal Boot&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp; 2&amp;nbsp; 1&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; &lt;/P&gt;&lt;P&gt;=&amp;gt; mmc rescan&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc dev&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;/P&gt;&lt;P&gt;mmc0(part 0) is current device&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc dev 2&lt;/P&gt;&lt;P&gt;CMD_SEND:0&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_NONE&lt;/P&gt;&lt;P&gt;CMD_SEND:8&lt;/P&gt;&lt;P&gt;ARG 0x000001AA&lt;/P&gt;&lt;P&gt;MMC_RSP_R1,5,6,7&amp;nbsp; 0x2F551248 &lt;/P&gt;&lt;P&gt;CMD_SEND:55&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_R1,5,6,7&amp;nbsp; 0x2F551248 &lt;/P&gt;&lt;P&gt;CMD_SEND:0&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_NONE&lt;/P&gt;&lt;P&gt;CMD_SEND:1&lt;/P&gt;&lt;P&gt;ARG 0x00000000&lt;/P&gt;&lt;P&gt;MMC_RSP_R3,4 0x00010000 &lt;/P&gt;&lt;P&gt;Card did not respond to voltage select!&lt;/P&gt;&lt;P&gt;mmc2(part 0) is current device&lt;/P&gt;&lt;P&gt;=&amp;gt; &amp;lt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had also defined CONFIG_MMC_TRACE to get more information about what was going on.&lt;/P&gt;&lt;P&gt;eMMC memory seems to be returning some responses, though I could not find what to make of them.&lt;/P&gt;&lt;P&gt;Does that mean there is no hardware issue since it returns these responses?&lt;/P&gt;&lt;P&gt;If so, what could be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 07:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-on-U-Boot-Card-did-not-respond-to-voltage-select/m-p/358704#M50303</guid>
      <dc:creator>durmus</dc:creator>
      <dc:date>2015-02-09T07:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC on U-Boot -- Card did not respond to voltage select!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-on-U-Boot-Card-did-not-respond-to-voltage-select/m-p/358705#M50304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durmuş&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can check responses from cmd1, it is described in&lt;/P&gt;&lt;P&gt;&lt;SPAN class="selected highlight"&gt;7.4.2&lt;/SPAN&gt;&amp;nbsp; Operating voltage range validation emmc 4.4 specification&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://rere.qmqm.pl/~mirq/JESD84-A44.pdf" title="http://rere.qmqm.pl/~mirq/JESD84-A44.pdf"&gt;http://rere.qmqm.pl/~mirq/JESD84-A44.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems this emmc does not support necessary voltages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 08:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-on-U-Boot-Card-did-not-respond-to-voltage-select/m-p/358705#M50304</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-09T08:51:45Z</dc:date>
    </item>
  </channel>
</rss>