<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックpreinstalled image setup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358296#M50248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am booting the ubuntu 12.04 preinstalled image from&lt;/P&gt;&lt;P&gt;&lt;A href="http://cdimage.ubuntu.com/releases/12.04/release/" title="http://cdimage.ubuntu.com/releases/12.04/release/"&gt;http://cdimage.ubuntu.com/releases/12.04/release/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;on my imx53 board but i cant complete it because&lt;/P&gt;&lt;P&gt;it cant detect the usb keyboard or mouse and when&lt;/P&gt;&lt;P&gt;it gets to system configuration screen for language&lt;/P&gt;&lt;P&gt;selection i cant make the selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there some setting i am missing or..&lt;BR /&gt;how can i get it to complete the setup??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Aug 2014 09:59:05 GMT</pubDate>
    <dc:creator>rayssadet</dc:creator>
    <dc:date>2014-08-14T09:59:05Z</dc:date>
    <item>
      <title>preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358296#M50248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am booting the ubuntu 12.04 preinstalled image from&lt;/P&gt;&lt;P&gt;&lt;A href="http://cdimage.ubuntu.com/releases/12.04/release/" title="http://cdimage.ubuntu.com/releases/12.04/release/"&gt;http://cdimage.ubuntu.com/releases/12.04/release/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;on my imx53 board but i cant complete it because&lt;/P&gt;&lt;P&gt;it cant detect the usb keyboard or mouse and when&lt;/P&gt;&lt;P&gt;it gets to system configuration screen for language&lt;/P&gt;&lt;P&gt;selection i cant make the selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there some setting i am missing or..&lt;BR /&gt;how can i get it to complete the setup??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 09:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358296#M50248</guid>
      <dc:creator>rayssadet</dc:creator>
      <dc:date>2014-08-14T09:59:05Z</dc:date>
    </item>
    <item>
      <title>Re: preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358297#M50249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rays&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;probably these images are not optimized for i.MX53 platform,&lt;/P&gt;&lt;P&gt;please check below i.MX53 Ubuntu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://eewiki.net/display/linuxonarm/i.MX53+Quick+Start#i.MX53QuickStart-Ubuntu14.04" title="http://eewiki.net/display/linuxonarm/i.MX53+Quick+Start#i.MX53QuickStart-Ubuntu14.04"&gt;http://eewiki.net/display/linuxonarm/i.MX53+Quick+Start#i.MX53QuickStart-Ubuntu14.04&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 10:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358297#M50249</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-14T10:08:13Z</dc:date>
    </item>
    <item>
      <title>Re: preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358298#M50250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how can i get an optimized one or maybe a way to optimize it&lt;/P&gt;&lt;P&gt;maybe by passing the language selection screen, it might load &lt;/P&gt;&lt;P&gt;the keyboard n mouse when it completely boots. &lt;BR /&gt;the name of the file is ubuntu-12.04-preinstalled-desktop-armhf+mx5.img.gz&lt;BR /&gt;with the mx5 in it i thought it will be ok ,,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Also i tried the instruction for ubuntu 14.04 above, that didnt even come on.&lt;/P&gt;&lt;P&gt;did you get it to run sometime... am not sure why ... the kernel seem high&lt;/P&gt;&lt;P&gt;though ..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also i tried the freescale &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;MX53_QSB_UBUNTU_SD_DEMO_IMAGE&lt;/A&gt; on win7&lt;/P&gt;&lt;P&gt;and it cant find any disk, not even my HDD..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a way i can get ubuntu on an sd card that will boot (preferably 12.04)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 10:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358298#M50250</guid>
      <dc:creator>rayssadet</dc:creator>
      <dc:date>2014-08-14T10:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358299#M50251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rays&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;optimized means that iomux settings were correctly set.&lt;/P&gt;&lt;P&gt;Regadring HDD I did not understood well, &lt;/P&gt;&lt;P&gt;i.MX53 Demo Image has document inside, which describes&lt;/P&gt;&lt;P&gt;what it supports and what not. Probably HDD is not supported.&lt;/P&gt;&lt;P&gt;In such case you should implement such support himself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 10:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358299#M50251</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-14T10:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358300#M50252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i mean my system hard disk drive HDD. The list to select destination drive is empty.&lt;/P&gt;&lt;P&gt;its just something.exe file that is suppose to create the boot sd card and nothing can&lt;/P&gt;&lt;P&gt;be done to modify it. its a select and click next kindda application.&lt;/P&gt;&lt;P&gt;am guessing there is no straight forward way to get ubuntu 12.04 to run on imx53&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on a side not, what do you make of this error:&lt;/P&gt;&lt;P&gt;GModule-CRITICAL **: g_module_close: 'module-&amp;gt;ref_count &amp;gt; 0' failed&lt;/P&gt;&lt;P&gt;Clutter-CRITICAL **: Unable to initialize Clutter: Failed to connected to any renderer due to constraints&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i get it when i try to run a program requiring libclutter-1.0 on the imx53&lt;/P&gt;&lt;P&gt;any insight is welcomed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;RAYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 11:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358300#M50252</guid>
      <dc:creator>rayssadet</dc:creator>
      <dc:date>2014-08-14T11:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: preinstalled image setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358301#M50253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rays&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is not desktop computer, but rather small chip,&lt;/P&gt;&lt;P&gt;so you can not expect that it will support everything&lt;/P&gt;&lt;P&gt;you can wish to attach.&lt;/P&gt;&lt;P&gt;I think first you should carefully read documentation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=IMX53_1109_LINUXDOCS_BUNDLE&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;IMX53_1109_LINUXDOCS_BUNDLE&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;MCIMX53-START-R i.MX53 QS Board Schematics&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then you may wish to run&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_MX53_1109_PATCH_IMAGE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and add step by step additional packages using&lt;/P&gt;&lt;P&gt;sources&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_11_09_ER_SOURCE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 15:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/preinstalled-image-setup/m-p/358301#M50253</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-14T15:47:29Z</dc:date>
    </item>
  </channel>
</rss>