<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Zero latency VPU h264 encoder with periodic intra frame support?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358182#M50231</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, and thank you for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you also confirm that the encoder doesn't support slice based encoding (or rather it does, but it can't output/input slices instead of full frames, so I need to wait for the full frame during the encoding and during the decoding, and I add 2 frames of latency to my application without considering anything else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Apr 2015 00:21:06 GMT</pubDate>
    <dc:creator>moire59</dc:creator>
    <dc:date>2015-04-08T00:21:06Z</dc:date>
    <item>
      <title>Zero latency VPU h264 encoder with periodic intra frame support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358178#M50227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The documentation is vague about it and there are no previous questions I could find.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this encoder profile supported from the imx6 platform?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 14:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358178#M50227</guid>
      <dc:creator>moire59</dc:creator>
      <dc:date>2015-03-27T14:45:18Z</dc:date>
    </item>
    <item>
      <title>Re: Zero latency VPU h264 encoder with periodic intra frame support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358179#M50228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you find a solution please let me know. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 16:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358179#M50228</guid>
      <dc:creator>gavingreenwalt</dc:creator>
      <dc:date>2015-03-27T16:13:12Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Zero latency VPU h264 encoder with periodic intra frame support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358180#M50229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, from this question: &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="311299" data-objecttype="1" href="https://community.freescale.com/thread/311299"&gt;https://community.freescale.com/thread/311299&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;and this quote from the manual:&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;intraRefresh where 0 = Intra MB refresh is not used. Otherwise = At least N MB's in every P-frame are encoded as intra MB's.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;It should be possible to have intra refresh P frames, while having maybe 1 I frame every few hours? Depending on how that number is declared? Even if it's a 16 bit one it should still be quite a lot of frames before an I one.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;But maybe my understanding of it is completely wrong.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 17:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358180#M50229</guid>
      <dc:creator>moire59</dc:creator>
      <dc:date>2015-03-27T17:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: Zero latency VPU h264 encoder with periodic intra frame support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358181#M50230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Giovanni,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct the intraRefresh parameter&amp;nbsp; is the latency and&amp;nbsp; you can control the I-frames and P-frames in the EncOpenParam structure, modifing the Gobsize &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typedef struct {&lt;/P&gt;&lt;P&gt;CodStd bitstreamFormat;&lt;/P&gt;&lt;P&gt;PhysicalAddress bitstreamBuffer;&lt;/P&gt;&lt;P&gt;Uint32 bitstreamBufferSize;&lt;/P&gt;&lt;P&gt;Uint8 *virt_bitstreamBuffer;&lt;/P&gt;&lt;P&gt;int streamBufResetEnable;&lt;/P&gt;&lt;P&gt;int picWidth;&lt;/P&gt;&lt;P&gt;int picHeight;&lt;/P&gt;&lt;P&gt;Uint32 frameRateInfo;&lt;/P&gt;&lt;P&gt;int bitRate;&lt;/P&gt;&lt;P&gt;int initialDelay;&lt;/P&gt;&lt;P&gt;int vbvBufferSize;&lt;/P&gt;&lt;P&gt;int enableAutoSkip;&lt;/P&gt;&lt;P&gt;int gopSize;&lt;/P&gt;&lt;P&gt;int sliceMode;&lt;/P&gt;&lt;P&gt;int sliceSizeMode;&lt;/P&gt;&lt;P&gt;int sliceSize;&lt;/P&gt;&lt;P&gt;int intraRefresh;&lt;/P&gt;&lt;P&gt;int sliceReport;&lt;/P&gt;&lt;P&gt;int mbReport;&lt;/P&gt;&lt;P&gt;int mbQpReport;&lt;/P&gt;&lt;P&gt;union {&lt;/P&gt;&lt;P&gt;EncMp4Param mp4Param;&lt;/P&gt;&lt;P&gt;EncH263Param h263Param;&lt;/P&gt;&lt;P&gt;EncAvcParam avcParam;&lt;/P&gt;&lt;P&gt;} EncStdParam;&lt;/P&gt;&lt;P&gt;} EncOpenParam;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gobsize &lt;/P&gt;&lt;P&gt;0 – Only first picture is I, 1 – all I pictures, 2 – IPIP…, 3 – IPPIPP…&lt;/P&gt;&lt;P&gt;The maximum value is limited by 60.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 21:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358181#M50230</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-04-07T21:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Zero latency VPU h264 encoder with periodic intra frame support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358182#M50231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, and thank you for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you also confirm that the encoder doesn't support slice based encoding (or rather it does, but it can't output/input slices instead of full frames, so I need to wait for the full frame during the encoding and during the decoding, and I add 2 frames of latency to my application without considering anything else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 00:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Zero-latency-VPU-h264-encoder-with-periodic-intra-frame-support/m-p/358182#M50231</guid>
      <dc:creator>moire59</dc:creator>
      <dc:date>2015-04-08T00:21:06Z</dc:date>
    </item>
  </channel>
</rss>