<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with usb audio capture in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357810#M50175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having problem in using arecord with the imx6 and an usb audio card.&lt;/P&gt;&lt;P&gt;It gives me "arecord: xrun:1387: read/write error, state = PREPARED".&lt;/P&gt;&lt;P&gt;Using dmesg, I can see that there is a "cannot submit datapipe for urb 0, error -28: not enough bandwidth" when the usb audio card is plugged in.&lt;/P&gt;&lt;P&gt;I am able to play audio to it using aplay.&lt;/P&gt;&lt;P&gt;My usb audio card is Usb Audio Class 2.0 compliant.&lt;/P&gt;&lt;P&gt;Using cat /proc/asound/card2/stream0, I can see that it has 2 channels and 1 endpoint for both playback and capture.&lt;/P&gt;&lt;P&gt;My Linux version is 3.0.35 and the Ubuntu version is 12.04.2 LTS&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Dec 2014 09:43:30 GMT</pubDate>
    <dc:creator>chyeminggan</dc:creator>
    <dc:date>2014-12-17T09:43:30Z</dc:date>
    <item>
      <title>Problem with usb audio capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357810#M50175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having problem in using arecord with the imx6 and an usb audio card.&lt;/P&gt;&lt;P&gt;It gives me "arecord: xrun:1387: read/write error, state = PREPARED".&lt;/P&gt;&lt;P&gt;Using dmesg, I can see that there is a "cannot submit datapipe for urb 0, error -28: not enough bandwidth" when the usb audio card is plugged in.&lt;/P&gt;&lt;P&gt;I am able to play audio to it using aplay.&lt;/P&gt;&lt;P&gt;My usb audio card is Usb Audio Class 2.0 compliant.&lt;/P&gt;&lt;P&gt;Using cat /proc/asound/card2/stream0, I can see that it has 2 channels and 1 endpoint for both playback and capture.&lt;/P&gt;&lt;P&gt;My Linux version is 3.0.35 and the Ubuntu version is 12.04.2 LTS&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 09:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357810#M50175</guid>
      <dc:creator>chyeminggan</dc:creator>
      <dc:date>2014-12-17T09:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with usb audio capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357811#M50176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems this is the same issue as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/311657"&gt;USB Audio errors on i.MX6 Quad&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 11:59:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357811#M50176</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-17T11:59:10Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with usb audio capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357812#M50177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configure your kernel with CONFIG_USB_EHCI_TT_NEWSCHED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Dec 2014 11:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357812#M50177</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-12-22T11:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with usb audio capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357813#M50178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a few problems compiling the kernel and finally got it working today.&lt;/P&gt;&lt;P&gt;Yup, enabling the CONFIG_USB_EHCI_TT_NEWSCHED solves the problem.&lt;/P&gt;&lt;P&gt;Thanks Igor and Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Dec 2014 07:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-with-usb-audio-capture/m-p/357813#M50178</guid>
      <dc:creator>chyeminggan</dc:creator>
      <dc:date>2014-12-29T07:58:32Z</dc:date>
    </item>
  </channel>
</rss>