<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX6S camera inputs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356746#M49960</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6S can handle two parallel camera inputs,&lt;/P&gt;&lt;P&gt;this is depicted on Figure 19-1. CSI2IPU gasket connectivity&lt;/P&gt;&lt;P&gt;Table 4-2. Muxing Options p.323 &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;In general also one can use usb cameras.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Feb 2015 00:47:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-02-09T00:47:31Z</dc:date>
    <item>
      <title>Question, i.MX6S camera inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356745#M49959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about camera input of i.MX6Solo.&lt;/P&gt;&lt;P&gt;Can i.MX6 Solo support two camera channels that are connected to parallel port CSI o i.MX6 Solo at the same time?&lt;/P&gt;&lt;P&gt;Referring to the schematics of i.MX6 SABRE AI Base board, we can find the AD7180 is used for two camera inputs and sending out to CSI0 parallel of i.MX6.&lt;/P&gt;&lt;P&gt;In the case of using one CSI parallel port of i.MX6S, can multiple camera streams be handled by i.MX6S?&lt;/P&gt;&lt;P&gt;If possible, how many camera inputs at the maximum can be handled in such case?&lt;/P&gt;&lt;P&gt;My customer wants to feed multiple camera data into i.MX6S and record the multiple streams to storage device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Feb 2015 09:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356745#M49959</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-02-08T09:43:35Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S camera inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356746#M49960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6S can handle two parallel camera inputs,&lt;/P&gt;&lt;P&gt;this is depicted on Figure 19-1. CSI2IPU gasket connectivity&lt;/P&gt;&lt;P&gt;Table 4-2. Muxing Options p.323 &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;In general also one can use usb cameras.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 00:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356746#M49960</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-09T00:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Question, i.MX6S camera inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356747#M49961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Please find the attached file for the block diagram around CSI input of the SABRE AI board.&lt;/P&gt;&lt;P&gt;On SABRE AI board, multiple cameras can be connected to CSI0 parallel port.&lt;/P&gt;&lt;P&gt;Maybe you are talking about the multiple camera inputs using different CSI port for each.&lt;/P&gt;&lt;P&gt;From the HW contracture of AI board, I think i.MX6Solo can handle multi camera data with single CSI parallel port.&lt;/P&gt;&lt;P&gt;Can I understand that i.MX6Solo can handle two camera inputs simultaneously?&lt;/P&gt;&lt;P&gt;And how many inputs at maximum can be handled with single CSI parallel port of i.MX6Solo?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 08:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356747#M49961</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-02-09T08:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S camera inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356748#M49962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miyamoto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I.MX6Solo can not handle multi camera data with single CSI parallel port,&lt;/P&gt;&lt;P&gt;i.MX6S can handle two parallel camera inputs connected to CSI0,1.&lt;/P&gt;&lt;P&gt;I am not ADV7180 expert, but I think ADV7180 can not work&lt;/P&gt;&lt;P&gt;with two cameras simultaneously. Only one camera can work at time.&lt;/P&gt;&lt;P&gt;I think you should contact Analog Devices with this question.&lt;/P&gt;&lt;P&gt;In genaral one can embed two camera streams to fpga and create&lt;/P&gt;&lt;P&gt;output stream as from one "virtual" camera and connect it to one CSI port.&lt;/P&gt;&lt;P&gt;Then one will have to parse cameras data from software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 09:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-camera-inputs/m-p/356748#M49962</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-09T09:01:02Z</dc:date>
    </item>
  </channel>
</rss>