<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion, i.MX283 LAN communication stops</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX283-LAN-communication-stops/m-p/356673#M49931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about unused pin handling of i.MX28.&lt;/P&gt;&lt;P&gt;My customer is using i.MX283 and he faces the issue that LAN communication could stop at EMC test.&lt;/P&gt;&lt;P&gt;The customer has a concern as below.&lt;/P&gt;&lt;P&gt;i.MX283 does not have some peripherals compared with i.MX287.&lt;/P&gt;&lt;P&gt;And some pins are supposed not to be connected to its die internally in i.MX283 chip, but the peripheral modules still exist on its die.&lt;/P&gt;&lt;P&gt;If so, some input pads are left as Open on its die, and those pads can be the antenna for noise.&lt;/P&gt;&lt;P&gt;Could you show me how user should treat the pins which is not used on i.MX283?&lt;/P&gt;&lt;P&gt;(Especially the pins which can be used on i.MX287 but not assigned on i.MX283)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 08 Feb 2015 09:19:03 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-02-08T09:19:03Z</dc:date>
    <item>
      <title>Question, i.MX283 LAN communication stops</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX283-LAN-communication-stops/m-p/356673#M49931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about unused pin handling of i.MX28.&lt;/P&gt;&lt;P&gt;My customer is using i.MX283 and he faces the issue that LAN communication could stop at EMC test.&lt;/P&gt;&lt;P&gt;The customer has a concern as below.&lt;/P&gt;&lt;P&gt;i.MX283 does not have some peripherals compared with i.MX287.&lt;/P&gt;&lt;P&gt;And some pins are supposed not to be connected to its die internally in i.MX283 chip, but the peripheral modules still exist on its die.&lt;/P&gt;&lt;P&gt;If so, some input pads are left as Open on its die, and those pads can be the antenna for noise.&lt;/P&gt;&lt;P&gt;Could you show me how user should treat the pins which is not used on i.MX283?&lt;/P&gt;&lt;P&gt;(Especially the pins which can be used on i.MX287 but not assigned on i.MX283)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Feb 2015 09:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX283-LAN-communication-stops/m-p/356673#M49931</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-02-08T09:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX283 LAN communication stops</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX283-LAN-communication-stops/m-p/356674#M49932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommendation not to connect on board such pins ("NC"),&lt;/P&gt;&lt;P&gt;which is not used on i.MX283. I am afraid there are no i.MX28&lt;/P&gt;&lt;P&gt;specific recommendations in case EMC test. For EMC one can&lt;/P&gt;&lt;P&gt;use general recommendations for shielding and protection&lt;/P&gt;&lt;P&gt;described in literature. Regarding acting pads as antenna, one can&lt;/P&gt;&lt;P&gt;try to set associated gpios as output with low level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 04:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX283-LAN-communication-stops/m-p/356674#M49932</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-02-09T04:55:23Z</dc:date>
    </item>
  </channel>
</rss>