<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 + CSI parallel camera + mxc capture driver + kernel 3.16 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355747#M49764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dennis, &lt;/P&gt;&lt;P&gt;did you found any solution for that ?&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Oct 2015 14:47:13 GMT</pubDate>
    <dc:creator>peterhafner</dc:creator>
    <dc:date>2015-10-21T14:47:13Z</dc:date>
    <item>
      <title>imx6 + CSI parallel camera + mxc capture driver + kernel 3.16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355744#M49761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi@all,&lt;/P&gt;&lt;P&gt;I'm using a custom board with an imx6DL and the kernel version 3.16! At the CSI0 interface I've an ADV7180 with a 8bit data connection!&lt;/P&gt;&lt;P&gt;I want to use the MXC v4l capture driver (VIDEO_MXC_CAPTURE) but this is using deprecated interface devices VIDEO_V4L2_INT_DEVICE.&lt;/P&gt;&lt;P&gt;I think the capture driver have to use the v4l2 sub devices (VIDEO_V4L2_SUBDEV_API)!?&lt;/P&gt;&lt;P&gt;If I try to activate the VIDEO_MXC_CAPTURE I got many linker errors, due to missing VIDEO_V4L2_INT_DEVICE components!&lt;/P&gt;&lt;P&gt;I think it could'nt be the right way to reactivate the deprecated VIDEO_V4L2_INT_DEVICE functionality, but I need an alternativ solution in the 3.16 kernel.&lt;/P&gt;&lt;P&gt;Is there any patch for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 07:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355744#M49761</guid>
      <dc:creator>DeLe</dc:creator>
      <dc:date>2015-03-04T07:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 + CSI parallel camera + mxc capture driver + kernel 3.16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355745#M49762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are other possibilities?&lt;/P&gt;&lt;P&gt;anyone?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2015 12:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355745#M49762</guid>
      <dc:creator>DeLe</dc:creator>
      <dc:date>2015-03-06T12:45:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 + CSI parallel camera + mxc capture driver + kernel 3.16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355746#M49763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;Have you checked if the issue is also included on the official Freescale release BSP? I’m afraid that we haven’t tested kernel 3.16, as the latest BSP release is L3.10.53 (Yocto project).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Hope this information will be useful for you. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Best regards! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;/Carlos&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2015 18:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355746#M49763</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-03-09T18:35:20Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 + CSI parallel camera + mxc capture driver + kernel 3.16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355747#M49764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dennis, &lt;/P&gt;&lt;P&gt;did you found any solution for that ?&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 14:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355747#M49764</guid>
      <dc:creator>peterhafner</dc:creator>
      <dc:date>2015-10-21T14:47:13Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 + CSI parallel camera + mxc capture driver + kernel 3.16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355748#M49765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Peter,&lt;/P&gt;&lt;P&gt;sorry for the late answer...&lt;/P&gt;&lt;P&gt;we didn't get a solution from community. So we improve the driver to support the newer SUBDEV_API interface.&lt;/P&gt;&lt;P&gt;Regards...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 07:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-parallel-camera-mxc-capture-driver-kernel-3-16/m-p/355748#M49765</guid>
      <dc:creator>DeLe</dc:creator>
      <dc:date>2016-01-04T07:59:05Z</dc:date>
    </item>
  </channel>
</rss>