<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Boot Configuration Select in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Configuration-Select/m-p/355661#M49756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, when EIM not used one can remove series resistors.&lt;/P&gt;&lt;P&gt;BT_CFG3 and BT_CFG4 pins can be connected to ground if&lt;/P&gt;&lt;P&gt;necessary. It is not recommended to left them unconnected due to&lt;/P&gt;&lt;P&gt;big internal pull resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Aug 2014 13:49:15 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-13T13:49:15Z</dc:date>
    <item>
      <title>Boot Configuration Select</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Configuration-Select/m-p/355660#M49755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am preparing a schematic which includes imx6 DualLite. I want to ask a question about Boot Configuration Selection.&lt;/P&gt;&lt;P&gt;In Sabre board, when BootMode0 = 0 and BootMode1 = 1, CPU decides Boot Config registers which are delegated from GPIO pins (EIM interface pins). I won't use EIM interface. I will put the same dipswitch (SW6) like SABRE. I don't want to put all series, pull down and pull up resistors like SABRE. My questions are:&lt;/P&gt;&lt;P&gt;* Are these series resistors (4.7K) necessary? I think this resistors are not necessary when I don't use EIM interface? Am I right?&lt;/P&gt;&lt;P&gt;* In SABRE board, BT_CFG3 and BT_CFG4 pins are pulled down via series resistors (4.7K) and 10K resistors. If I don't use these pins, can I connect them directly to the GND or left open? If yes, which one is more meaningful?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Aug 2014 11:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Configuration-Select/m-p/355660#M49755</guid>
      <dc:creator>muratünal</dc:creator>
      <dc:date>2014-08-13T11:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Configuration Select</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Configuration-Select/m-p/355661#M49756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, when EIM not used one can remove series resistors.&lt;/P&gt;&lt;P&gt;BT_CFG3 and BT_CFG4 pins can be connected to ground if&lt;/P&gt;&lt;P&gt;necessary. It is not recommended to left them unconnected due to&lt;/P&gt;&lt;P&gt;big internal pull resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Aug 2014 13:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Configuration-Select/m-p/355661#M49756</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-13T13:49:15Z</dc:date>
    </item>
  </channel>
</rss>