<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックdev-pkgs tools-sdk in nitrogen6x build</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/dev-pkgs-tools-sdk-in-nitrogen6x-build/m-p/355134#M49667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build for my sabrelite board in Yocto (using machine nitrogen6x).&lt;/P&gt;&lt;P&gt;I'm trying to include the gcc compile, tools etc., so I add following lines in my local.conf file&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += " \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; dev-pkgs \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; tools-sdk \&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I get an error when I compile with this features (using core-image-base image):&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: package libxml-parser-perl contains bad RPATH ...../build/tmp/sysroots/nitrogen6x/usr/lib in file ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/packages-split/libxml-parser-perl/usr/lib/perl/vendor_perl/5.14.3/auto/XML/Parser/Expat/Expat.so&lt;/P&gt;&lt;P&gt;ERROR: QA run found fatal errors. Please consider fixing them.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_package_qa&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/temp/log.do_package.11612&lt;/P&gt;&lt;P&gt;ERROR: Task 2598 (...../sources/poky/meta/recipes-devtools/perl/libxml-parser-perl_2.41.bb, do_package) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I'm missing here?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Sep 2014 22:08:26 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2014-09-29T22:08:26Z</dc:date>
    <item>
      <title>dev-pkgs tools-sdk in nitrogen6x build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dev-pkgs-tools-sdk-in-nitrogen6x-build/m-p/355134#M49667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build for my sabrelite board in Yocto (using machine nitrogen6x).&lt;/P&gt;&lt;P&gt;I'm trying to include the gcc compile, tools etc., so I add following lines in my local.conf file&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += " \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; dev-pkgs \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; tools-sdk \&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I get an error when I compile with this features (using core-image-base image):&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: package libxml-parser-perl contains bad RPATH ...../build/tmp/sysroots/nitrogen6x/usr/lib in file ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/packages-split/libxml-parser-perl/usr/lib/perl/vendor_perl/5.14.3/auto/XML/Parser/Expat/Expat.so&lt;/P&gt;&lt;P&gt;ERROR: QA run found fatal errors. Please consider fixing them.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_package_qa&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/temp/log.do_package.11612&lt;/P&gt;&lt;P&gt;ERROR: Task 2598 (...../sources/poky/meta/recipes-devtools/perl/libxml-parser-perl_2.41.bb, do_package) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I'm missing here?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 22:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dev-pkgs-tools-sdk-in-nitrogen6x-build/m-p/355134#M49667</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-09-29T22:08:26Z</dc:date>
    </item>
  </channel>
</rss>