<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic WinCE7 + Silverlight on Sabre in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168051#M4954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi I wrote a test app for using Silverlight on WinCE7. The app implements an animation of moving a button using a storyboard whenever the button is clicked. However the app doesn't work like it should. On a button click the button is supposed to move over 8 secs in a manner given below  Sec 1 BUTTON 2 BUTTON 3 BUTTON 4 BUTTON 5 BUTTON 6 BUTTON 7 BUTTON 8 BUTTON  However immediately after the button is clicked the window goes blank. The button then appears after 8 secs The CPU usage jumps from 3% to 30% for those 8 secs (checked using Performance Monitor tool) Why is it that the smooth animation of the button moving is not displayed? Are there any settings that I need to enable?  Warm Regards Will&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jun 2012 09:14:52 GMT</pubDate>
    <dc:creator>WILBURCOLACO</dc:creator>
    <dc:date>2012-06-12T09:14:52Z</dc:date>
    <item>
      <title>WinCE7 + Silverlight on Sabre</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168051#M4954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi I wrote a test app for using Silverlight on WinCE7. The app implements an animation of moving a button using a storyboard whenever the button is clicked. However the app doesn't work like it should. On a button click the button is supposed to move over 8 secs in a manner given below  Sec 1 BUTTON 2 BUTTON 3 BUTTON 4 BUTTON 5 BUTTON 6 BUTTON 7 BUTTON 8 BUTTON  However immediately after the button is clicked the window goes blank. The button then appears after 8 secs The CPU usage jumps from 3% to 30% for those 8 secs (checked using Performance Monitor tool) Why is it that the smooth animation of the button moving is not displayed? Are there any settings that I need to enable?  Warm Regards Will&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 09:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168051#M4954</guid>
      <dc:creator>WILBURCOLACO</dc:creator>
      <dc:date>2012-06-12T09:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE7 + Silverlight on Sabre</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168052#M4955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;the button is supposed to move as given below ....BUTTON ........BUTTON ............BUTTON ................BUTTON ................BUTTON ............BUTTON ........BUTTON ....BUTTON&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 09:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168052#M4955</guid>
      <dc:creator>WILBURCOLACO</dc:creator>
      <dc:date>2012-06-12T09:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE7 + Silverlight on Sabre</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168053#M4956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wilbur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What does your Native C++ code button animation code look like under your VS2008 look like? This is probably why there is no animation of the button.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2012 15:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE7-Silverlight-on-Sabre/m-p/168053#M4956</guid>
      <dc:creator>iMXAndrew</dc:creator>
      <dc:date>2012-06-27T15:19:58Z</dc:date>
    </item>
  </channel>
</rss>