<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX28: Get Boot Mode from ROM loader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354284#M49493</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to read from the second stage bootloader which boot mode the &lt;SPAN style="font-size: 13.3333330154419px;"&gt;ROM loader &lt;/SPAN&gt;used to boot the device, especially to distinguish if it was booted by USB recovery or NAND boot mode. Reading the Boot Mode Pads is not reliable since the Boot Mode Pads can be already released (eg, BM2 to force from NAND to USB recovery mode) when the bootloader reads the pin values (high or low).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any register, I didn't find one in the manual, which holds the boot mode at power-up? Or is there any other way to obtain the boot mode at power-up state?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jörg Krause&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2015 16:28:27 GMT</pubDate>
    <dc:creator>jörg_krause</dc:creator>
    <dc:date>2015-03-26T16:28:27Z</dc:date>
    <item>
      <title>i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354284#M49493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to read from the second stage bootloader which boot mode the &lt;SPAN style="font-size: 13.3333330154419px;"&gt;ROM loader &lt;/SPAN&gt;used to boot the device, especially to distinguish if it was booted by USB recovery or NAND boot mode. Reading the Boot Mode Pads is not reliable since the Boot Mode Pads can be already released (eg, BM2 to force from NAND to USB recovery mode) when the bootloader reads the pin values (high or low).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any register, I didn't find one in the manual, which holds the boot mode at power-up? Or is there any other way to obtain the boot mode at power-up state?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jörg Krause&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 16:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354284#M49493</guid>
      <dc:creator>jörg_krause</dc:creator>
      <dc:date>2015-03-26T16:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354285#M49494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jörg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right - there is no register preserving&amp;nbsp; power-up boot mode.&lt;/P&gt;&lt;P&gt;Seems one can add small routine in bootlets (at power initialization)&lt;/P&gt;&lt;P&gt;reading boot pins and storing them somewhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 00:06:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354285#M49494</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-30T00:06:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354286#M49495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;many thanks for your reply! Reading boot pins does not work in all cases for USB recovery boot mode. If the recovery button, e.g. BM2 for switching from NAND to USB boot, is pressed and the USB is connected the ROM loader starts in USB recovery boot mode. Now, the button is released and afterwards a BootStream image (bootlets) is loaded by the ROM loader. If the bootlet now reads the boot pins, the pins do not have the same state as they had when the ROM loader read the pins, because the button was released and so BM2 is not low anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jörg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 11:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354286#M49495</guid>
      <dc:creator>jörg_krause</dc:creator>
      <dc:date>2015-03-30T11:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354287#M49496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jörg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for USB usage in recovery boot mode one can check USB settings, like&lt;/P&gt;&lt;P&gt;HW_USBPHY_CTRL[CLKGATE]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 15:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354287#M49496</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-30T15:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354288#M49497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Checking the USB-PHY registers helps to distinguish between NAND boot mode and USB recovery boot mode, but it seems more like a workaround.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a U-Boot version from Timesys for i.MX28EVK I've found a comment that the ROM loader stores the boot mode at the fixed address 0x00019BF0 in OCRAM. I've checked this and it seems correct. Reading this address after power-up shows 0x0 for USB boot mode and 0x4 for NAND boot mode. Is this documented somewhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jörg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2015 08:11:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354288#M49497</guid>
      <dc:creator>jörg_krause</dc:creator>
      <dc:date>2015-04-01T08:11:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28: Get Boot Mode from ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354289#M49498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am afraid not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 02:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Get-Boot-Mode-from-ROM-loader/m-p/354289#M49498</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-02T02:30:33Z</dc:date>
    </item>
  </channel>
</rss>