<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX6Q ECSPI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353925#M49385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SS should be used in slave mode as describes&lt;/P&gt;&lt;P&gt;sect.21.4.2 Slave Mode&amp;nbsp; &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this configuration, Chip Select (SS) becomes an input signal, and is used to control&lt;/P&gt;&lt;P&gt;data transfers through the Shift register, as well as to load/store the data FIFO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also below one can find slave mode usage examples&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-97380"&gt;i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/334511"&gt;i.MX6 SPI Slave mode&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 Jan 2015 15:09:54 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-18T15:09:54Z</dc:date>
    <item>
      <title>Question, i.MX6Q ECSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353924#M49384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer is facing the issue that ECSPI module of i.MX6Q cannot communicate with a external SPI device on their proto-board.&lt;/P&gt;&lt;P&gt;They use i.MX6Q ECSPI as slave and the external device is the master.&lt;/P&gt;&lt;P&gt;Because the external device is the only SPI device, they do not use SS.&lt;/P&gt;&lt;P&gt;The SS pin of i.MX6 is open.&lt;/P&gt;&lt;P&gt;The customer’s configuration is as below.&lt;/P&gt;&lt;P&gt;ECSPI5_CONREG = 0x0170_D101&lt;/P&gt;&lt;P&gt;ECSPI5_CONFREG = 0x0000_0001&lt;/P&gt;&lt;P&gt;ECSPI5_INTREG = 0x0000_0028&lt;/P&gt;&lt;P&gt;ECSPI5_DMAREG = 0x0000_0000&lt;/P&gt;&lt;P&gt;ECSPI5_STATREG = 0x0000_0003&lt;/P&gt;&lt;P&gt;Could you give me advice on the cause of this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jan 2015 14:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353924#M49384</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-01-18T14:36:58Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q ECSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353925#M49385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SS should be used in slave mode as describes&lt;/P&gt;&lt;P&gt;sect.21.4.2 Slave Mode&amp;nbsp; &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this configuration, Chip Select (SS) becomes an input signal, and is used to control&lt;/P&gt;&lt;P&gt;data transfers through the Shift register, as well as to load/store the data FIFO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also below one can find slave mode usage examples&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-97380"&gt;i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/334511"&gt;i.MX6 SPI Slave mode&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jan 2015 15:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353925#M49385</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-18T15:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q ECSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353926#M49386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your prompt reply.&lt;/P&gt;&lt;P&gt;Can I understand that SS pin of i.MX6 should be connected to external device even if the SPI is used for peer-to-peer communication?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jan 2015 01:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353926#M49386</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-01-19T01:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q ECSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353927#M49387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miyamoto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes SS pin of i.MX6 should be connected to external device&lt;/P&gt;&lt;P&gt;even if the SPI is used for peer-to-peer communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jan 2015 11:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-ECSPI/m-p/353927#M49387</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-19T11:26:38Z</dc:date>
    </item>
  </channel>
</rss>