<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 USB Host RX Errors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-RX-Errors/m-p/353816#M49378</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear experts -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing a perplexing issue with USB stability. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6 Solo board with USB Host. I'm running Linux 3.0.101.&lt;/P&gt;&lt;P&gt;The USB port works well with Mass storage device, web cam, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have another USB camera that works well on a PC, but when connected to our board gives a low frame-rate.&lt;/P&gt;&lt;P&gt;In the USB PHY registers I can see UTMI_RXERROR_FAIL_COUNT increasing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried - &lt;/P&gt;&lt;P&gt;(1) Several cameras&lt;/P&gt;&lt;P&gt;(2) Replacing the USB cable (several types)&lt;/P&gt;&lt;P&gt;(3) Shortening the cable&lt;/P&gt;&lt;P&gt;(4) Soldering the cable directly to our board.&lt;/P&gt;&lt;P&gt;(5) Several boards.&lt;/P&gt;&lt;P&gt;(6) Some electrical tweaks, etc... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every time I see varying performance and error levels.... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any ideas what else I could try or what might be the source of the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2015 12:37:13 GMT</pubDate>
    <dc:creator>erezsteinberg</dc:creator>
    <dc:date>2015-03-26T12:37:13Z</dc:date>
    <item>
      <title>USB Host RX Errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-RX-Errors/m-p/353816#M49378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear experts -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing a perplexing issue with USB stability. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6 Solo board with USB Host. I'm running Linux 3.0.101.&lt;/P&gt;&lt;P&gt;The USB port works well with Mass storage device, web cam, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have another USB camera that works well on a PC, but when connected to our board gives a low frame-rate.&lt;/P&gt;&lt;P&gt;In the USB PHY registers I can see UTMI_RXERROR_FAIL_COUNT increasing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried - &lt;/P&gt;&lt;P&gt;(1) Several cameras&lt;/P&gt;&lt;P&gt;(2) Replacing the USB cable (several types)&lt;/P&gt;&lt;P&gt;(3) Shortening the cable&lt;/P&gt;&lt;P&gt;(4) Soldering the cable directly to our board.&lt;/P&gt;&lt;P&gt;(5) Several boards.&lt;/P&gt;&lt;P&gt;(6) Some electrical tweaks, etc... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every time I see varying performance and error levels.... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any ideas what else I could try or what might be the source of the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 12:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-RX-Errors/m-p/353816#M49378</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2015-03-26T12:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB Host RX Errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-RX-Errors/m-p/353817#M49379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can tweak receiver side using sect.4.3.3.3 Receiver settings—&lt;/P&gt;&lt;P&gt;USBPHY_RX register &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4589.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4589&lt;/A&gt; Configuring USB on i.MX 6 Series Processors&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also recommended to check layout rules with sect.&lt;/P&gt;&lt;P&gt;3.11 USB recommendations &lt;A href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQ6SDLHDG&lt;/A&gt; &lt;/P&gt;&lt;P&gt;IMX6DQ6SDLHDG, Hardware Development Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Apr 2015 14:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-RX-Errors/m-p/353817#M49379</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-05T14:13:25Z</dc:date>
    </item>
  </channel>
</rss>