<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX23 Boot from SD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353694#M49360</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Okay, how exactly do I write to the OTP memory? Can I use the debug UART or USB? I haven't been able to find this in the documentation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jan 2015 17:26:40 GMT</pubDate>
    <dc:creator>johnsullivan</dc:creator>
    <dc:date>2015-01-20T17:26:40Z</dc:date>
    <item>
      <title>I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353690#M49356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm developing a board using the I.MX23 and I want to boot from an SD Card. Do I need to write anything to the OTP memory to do this?&lt;/P&gt;&lt;P&gt;I am confused about the default behavior of the SD_POWER_GATE_GPIO and SD_POWER_UP_DELAY. Do most SD card require a power up delay? Or would I be fine without it? This board is for my own education so it does not need to be very robust.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Jan 2015 21:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353690#M49356</guid>
      <dc:creator>johnsullivan</dc:creator>
      <dc:date>2015-01-17T21:08:40Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353691#M49357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi john&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;two OTP bit fields in HW_OCOTP_ROM0 should be burned for SD boot:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. SD_MBR_BOOT &lt;/P&gt;&lt;P&gt;2. SD_POWER_GATE_GPIO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bitburner can be used during development. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX233&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OTP_TOOLS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : A set of tools for managing OTP bits on the i.MX23 and i.MX28.&lt;/P&gt;&lt;P&gt;Contains BitBurner.exe, the otp_burner.py and BitInit.exe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jan 2015 15:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353691#M49357</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-18T15:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353692#M49358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it required that I burn any values? It would be much simpler if I don't have to write anything to the OTP memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jan 2015 17:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353692#M49358</guid>
      <dc:creator>johnsullivan</dc:creator>
      <dc:date>2015-01-19T17:21:41Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353693#M49359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for OTP values please read Reference Manual.&lt;/P&gt;&lt;P&gt;Unfortunately it would not be simpler for you without &lt;/P&gt;&lt;P&gt;write anything to the OTP memory&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 01:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353693#M49359</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-20T01:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353694#M49360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Okay, how exactly do I write to the OTP memory? Can I use the debug UART or USB? I haven't been able to find this in the documentation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 17:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353694#M49360</guid>
      <dc:creator>johnsullivan</dc:creator>
      <dc:date>2015-01-20T17:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX23 Boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353695#M49361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bitburner can be used to write to the OTP memory &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX233&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" target="_blank"&gt;IMX_OTP_TOOLS&lt;/A&gt; &lt;A href="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif"&gt;&lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/A&gt; : A set of tools for managing OTP bits on the i.MX23 and i.MX28.&lt;/P&gt;&lt;P&gt;Contains BitBurner.exe, the otp_burner.py and BitInit.exe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2015 02:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/353695#M49361</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-21T02:50:04Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/1136124#M161137</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 15:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX23-Boot-from-SD/m-p/1136124#M161137</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T15:16:13Z</dc:date>
    </item>
  </channel>
</rss>