<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックInterrupt in UART for Transmit and receive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interrupt-in-UART-for-Transmit-and-receive/m-p/353426#M49296</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am working on UART driver for sabrelite IMX6DQ board in QNX neutrino 6.6.I am not using the resource manager available&lt;/P&gt;&lt;P&gt; in the BSP but creating a seperate driver with using the io-char framework.I am trying to do the transmit and receive &lt;/P&gt;&lt;P&gt;with the interrupts but i am not able to get any interrupts for the receive and getting only one interrupt for the &lt;/P&gt;&lt;P&gt;trasmit for the first time alone and then i am not getting any interrupts for the trasmit also.&lt;/P&gt;&lt;P&gt;I am using the interruptattach method for doing the interrupt registration.In the ISR i am not able to do the &lt;/P&gt;&lt;P&gt;interruptUnmask as it crashes the application at the call of the interruptattach function itself.I am also not able to &lt;/P&gt;&lt;P&gt;have NULL return as it also crashes the application at initialisation itself.&lt;/P&gt;&lt;P&gt;I have been able to do the transmit and receive with the polling method where in it was possible with the polling for &lt;/P&gt;&lt;P&gt;the TXEMPTY and the RXEMPTY bits of the test register.But the same is not working for the polling of the Status bits of &lt;/P&gt;&lt;P&gt;the status register for the trasmit and receive.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am attaching my code for reference kindly help me out in finding the bug in the code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Oct 2014 05:50:23 GMT</pubDate>
    <dc:creator>praveenkumarvs</dc:creator>
    <dc:date>2014-10-27T05:50:23Z</dc:date>
    <item>
      <title>Interrupt in UART for Transmit and receive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interrupt-in-UART-for-Transmit-and-receive/m-p/353426#M49296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am working on UART driver for sabrelite IMX6DQ board in QNX neutrino 6.6.I am not using the resource manager available&lt;/P&gt;&lt;P&gt; in the BSP but creating a seperate driver with using the io-char framework.I am trying to do the transmit and receive &lt;/P&gt;&lt;P&gt;with the interrupts but i am not able to get any interrupts for the receive and getting only one interrupt for the &lt;/P&gt;&lt;P&gt;trasmit for the first time alone and then i am not getting any interrupts for the trasmit also.&lt;/P&gt;&lt;P&gt;I am using the interruptattach method for doing the interrupt registration.In the ISR i am not able to do the &lt;/P&gt;&lt;P&gt;interruptUnmask as it crashes the application at the call of the interruptattach function itself.I am also not able to &lt;/P&gt;&lt;P&gt;have NULL return as it also crashes the application at initialisation itself.&lt;/P&gt;&lt;P&gt;I have been able to do the transmit and receive with the polling method where in it was possible with the polling for &lt;/P&gt;&lt;P&gt;the TXEMPTY and the RXEMPTY bits of the test register.But the same is not working for the polling of the Status bits of &lt;/P&gt;&lt;P&gt;the status register for the trasmit and receive.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am attaching my code for reference kindly help me out in finding the bug in the code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 05:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interrupt-in-UART-for-Transmit-and-receive/m-p/353426#M49296</guid>
      <dc:creator>praveenkumarvs</dc:creator>
      <dc:date>2014-10-27T05:50:23Z</dc:date>
    </item>
  </channel>
</rss>