<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PCIe problem on SabreSD with kernel 3.10.17</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353042#M49213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at below links with working PCIe on 3.10.17&lt;/P&gt;&lt;P&gt;(on first one can find configs)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/320124"&gt;pcie "phy link never came up" on sabresd running dora 3.10.17_beta&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/425265"&gt;Re: PCIe host controller driver in 3.10.17 kernel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Mar 2015 12:02:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-03-04T12:02:00Z</dc:date>
    <item>
      <title>PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353037#M49208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to get PCIe to work on SabreSD. The PCI device is the Exar XR17V35 eval. board. The root is detected but the device is not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel is 3.10.17-1.0.1_ga and there is no PCI enabled in U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probing the signals I find that the power and reset signals toggle as expected, but there is no reference clock at all (so no wonder the phy link does not come up).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# dmesg | grep pci&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: scanning bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: supports D1&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# disabled&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: fixups for bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: scanning bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: fixups for bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: fixup irq: got 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: assigning IRQ 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 4 [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 5 [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;ehci-pci: EHCI PCI platform driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Clocks (/sys/kernel/debug/clk) - the 125 MHz clock is what I would expect:&lt;/P&gt;&lt;P&gt;pcie_axi_sel&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; axi&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp; 264000000&lt;/P&gt;&lt;P&gt;pcie_axi&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pcie_axi_sel&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp; 264000000&lt;/P&gt;&lt;P&gt;pcie_ref&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pll6_enet&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp; 125000000&lt;/P&gt;&lt;P&gt;pcie_ref_125m&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pcie_ref&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp; 125000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel config:&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;# Bus support&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;CONFIG_PCI=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_DOMAINS=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_SYSCALL=y&lt;/P&gt;&lt;P&gt;CONFIG_ARCH_SUPPORTS_MSI=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_MSI=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_DEBUG=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_STUB=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_ATS=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_IOV=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;# PCI host controller drivers&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;CONFIG_PCIE_DW=y&lt;/P&gt;&lt;P&gt;CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;CONFIG_PCIEPORTBUS=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;CONFIG_PCIEAER=y&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;CONFIG_PCIEASPM=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;CONFIG_PCIEASPM_DEFAULT=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;CONFIG_PCIE_PME=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions as to what I am missing? Is my SabreSD board faulty?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to add PCI support to U-Boot 2014.01, I tried the kernel 3.0.35 but to no avail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2015 12:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353037#M49208</guid>
      <dc:creator>lmhdoms</dc:creator>
      <dc:date>2015-03-03T12:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353038#M49209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hilmhdoms&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;suggest to set configuration as described in attached&lt;/P&gt;&lt;P&gt;document sect.42.4 Using PCIe Endpoint and Running Tests&lt;/P&gt;&lt;P&gt;and add Exar XR17V3x drivers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/exoter-rover/drivers-exar_pcie_uart" title="https://github.com/exoter-rover/drivers-exar_pcie_uart"&gt;exoter-rover/drivers-exar_pcie_uart · GitHub&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid PCIe is not supported in U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 01:14:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353038#M49209</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-04T01:14:23Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353039#M49210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer. I checked the ref. manual and don't see anything I need to do - I am not enabling the EP mode, which I believe is correct... As for the Exar driver I got the latest from Exar, but as long as the PCI link is not established, the driver can't be the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have PCIe working on the SabreSD board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 08:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353039#M49210</guid>
      <dc:creator>lmhdoms</dc:creator>
      <dc:date>2015-03-04T08:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353040#M49211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;description in document is not about enabling the EP mode,&lt;/P&gt;&lt;P&gt;could you confirm that defconfig has:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale i.MX6 PCIe controller&lt;/P&gt;&lt;P&gt;-&amp;gt; Bus support&lt;/P&gt;&lt;P&gt;-&amp;gt; PCI host controller drivers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 08:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353040#M49211</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-04T08:32:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353041#M49212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Please see the initial post, I listed which PCI options are enabled in my .config file. There are both bus support and host controller entries, are they what you are asking for?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 09:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353041#M49212</guid>
      <dc:creator>lmhdoms</dc:creator>
      <dc:date>2015-03-04T09:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353042#M49213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at below links with working PCIe on 3.10.17&lt;/P&gt;&lt;P&gt;(on first one can find configs)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/320124"&gt;pcie "phy link never came up" on sabresd running dora 3.10.17_beta&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/425265"&gt;Re: PCIe host controller driver in 3.10.17 kernel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 12:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353042#M49213</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-04T12:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353043#M49214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already studied those posts, but don't think they help me. However, I understand that it is correct not to enable RC and EP, and also to have correct clock termination resistors, which should be the case on my SabreSD board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 12:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353043#M49214</guid>
      <dc:creator>lmhdoms</dc:creator>
      <dc:date>2015-03-04T12:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353044#M49215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class="replyToName"&gt;lmhdoms,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;is the ref board mini PCIe or are you using adaptors ? I had lots of trouble with adaptors and instrumented the imx6_pcie_link_up function with printk in linux 3.10.17 (drivers/pci/host/pci-imx6.c) to see what happened. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;In my case, it turned out that the link quality was too bad. Your log message "phy link never came up" might indicate similar issues. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Frank&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;H5 class="simple"&gt;&lt;/H5&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 21:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353044#M49215</guid>
      <dc:creator>frankba</dc:creator>
      <dc:date>2015-03-04T21:16:13Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353045#M49216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a photo of the boards, we use an adaptor GH-EMLX1 between SabreSD and the Exar board. The Exar board and adaptor is tested OK on an x86 SBC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The register PMU_MISC1n (0x020C8160) is: 8000 040B, which enables output buffer and PCIe clock for LVDS1. I guess it is ok, yet no clock appears.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51026i6ED9FF63B35AF3B7/image-size/large?v=v2&amp;amp;px=999" title="2015-03-05 09.14.48.jpg" alt="2015-03-05 09.14.48.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 09:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353045#M49216</guid>
      <dc:creator>lmhdoms</dc:creator>
      <dc:date>2015-03-05T09:48:18Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe problem on SabreSD with kernel 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353046#M49217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt; I have connected a mini PCIE based WLAN module on sabre SD board and got it working.&lt;/P&gt;&lt;P&gt; Initially i faced some problem but after that it worked. &lt;/P&gt;&lt;P&gt; Is it the 100MHZ clock which is not coming in your case?&lt;/P&gt;&lt;P&gt; Can you Check "&amp;nbsp; MPCIE_3V3 " Volatge on the Sabre board after connecting the EXAR board with it.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 05:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-problem-on-SabreSD-with-kernel-3-10-17/m-p/353046#M49217</guid>
      <dc:creator>sumit8915</dc:creator>
      <dc:date>2015-07-01T05:39:15Z</dc:date>
    </item>
  </channel>
</rss>