<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to write eMMC with 'dd' command in linux? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-write-eMMC-with-dd-command-in-linux/m-p/352460#M49071</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it is possible, for example attached Linux Guide sect.8.3&lt;/P&gt;&lt;P&gt;shows such operations for both SD/eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2015 08:20:54 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-03-26T08:20:54Z</dc:date>
    <item>
      <title>Is it possible to write eMMC with 'dd' command in linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-write-eMMC-with-dd-command-in-linux/m-p/352459#M49070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use i.MX6 SABRE-SDP board.&lt;/P&gt;&lt;P&gt;I want to know whether writing eMMC is possible after booting from SD card slot or NFS.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 07:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-write-eMMC-with-dd-command-in-linux/m-p/352459#M49070</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-03-26T07:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to write eMMC with 'dd' command in linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-write-eMMC-with-dd-command-in-linux/m-p/352460#M49071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it is possible, for example attached Linux Guide sect.8.3&lt;/P&gt;&lt;P&gt;shows such operations for both SD/eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 08:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-write-eMMC-with-dd-command-in-linux/m-p/352460#M49071</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-03-26T08:20:54Z</dc:date>
    </item>
  </channel>
</rss>