<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Mini PCIe module and additional ethernet questions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352207#M49023</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can&lt;/P&gt;&lt;P&gt;attach different PCIe cards and try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Aug 2014 14:08:03 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-28T14:08:03Z</dc:date>
    <item>
      <title>Mini PCIe module and additional ethernet questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352204#M49020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I recently bought i.MX6 Sabre BOARD with quad-core processor (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;tid=vanSABRESDB"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;tid=vanSABRESDB&lt;/A&gt;&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;BR /&gt;The purpose of buying the board is learning at first place, because I'm new in embedded world.&lt;/P&gt;&lt;P&gt;Currently I'm running Ubuntu 14.04 with kernel 3.15.8-armv7-x5. My questions are as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) Is it possible to implement second ethernet adapter on the board? My intention is to have two different subnets, first for internet access and second for internal purposes.&lt;/P&gt;&lt;P&gt;2.) I need a recommendation for mini PCIe half-size 3G module that I could use on the board? Is there any model which was confirmed as linux supported?&lt;/P&gt;&lt;P&gt;3.) Can I use the same slot for mini PCIe wireless module? Is there any recommendation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Nenad &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Aug 2014 08:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352204#M49020</guid>
      <dc:creator>nenadstojanovic</dc:creator>
      <dc:date>2014-08-12T08:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe module and additional ethernet questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352205#M49021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nenad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. yes, for example i.MX_6Dual6Quad_Sabre-SD_Linux_Release_Notes.pdf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; states that was tested&amp;nbsp;&amp;nbsp;&amp;nbsp; Intel gigabit CT network standard PCIE GEN1 X1 card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; I am not aware of tested 3G modules. In general any standard PCIe module will work&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for example below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.option.com/product/gtm671wgtm679w/specifications" title="http://www.option.com/product/gtm671wgtm679w/specifications"&gt;GTM671W/GTM679W | Option&lt;/A&gt;&lt;/P&gt;&lt;P class="active_link"&gt;&lt;/P&gt;&lt;P class="active_link"&gt;3. You can not attach two different modules to one slot, as for WiFi&lt;/P&gt;&lt;P class="active_link"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; i.MX_6Dual6Quad_Sabre-SD_Linux_Release_Notes.pdf&lt;/P&gt;&lt;P class="active_link"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; states that was tested&lt;/P&gt;&lt;P class="active_link"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; iwl5100/6300 WiFi mini-PCIE GEN1 X1 cards.&lt;/P&gt;&lt;P class="active_link"&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Aug 2014 02:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352205#M49021</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-13T02:00:51Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe module and additional ethernet questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352206#M49022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it possible to connect some other Mini PCIe card instead of 3G card on the Mini PCIe slot on the Sabre SDB? Can I connect Mini PCIe Ethernet card or Mini PCIe Wireless card instead of 3g card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nedeljko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 09:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352206#M49022</guid>
      <dc:creator>nedeljkoradulov</dc:creator>
      <dc:date>2014-08-28T09:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe module and additional ethernet questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352207#M49023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can&lt;/P&gt;&lt;P&gt;attach different PCIe cards and try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 14:08:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mini-PCIe-module-and-additional-ethernet-questions/m-p/352207#M49023</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-28T14:08:03Z</dc:date>
    </item>
  </channel>
</rss>