<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Reset PLL2 and PLL3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352113#M48992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLL2 usually is used for DDR (MMDC module), so if program&lt;/P&gt;&lt;P&gt;runs from DDR, it is not possible to change clock (or source of clock)&lt;/P&gt;&lt;P&gt;of MMDC module. One needs to put DDR to self-refresh, jump to iRAM,&lt;/P&gt;&lt;P&gt;switch/change clocks for MMDC, then return to normal operation from DDR.&lt;/P&gt;&lt;P&gt;In general also crash can be caused by PFD gating, described in&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/eng_bulletin/EB790.pdf?fasp=1&amp;amp;WT_TYPE=Engineering%20Bulletins&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;EB790&lt;/A&gt; Configuration of Phase Fractional Dividers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Dec 2014 00:59:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-16T00:59:02Z</dc:date>
    <item>
      <title>Reset PLL2 and PLL3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352112#M48991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CPU boots from DDR Ram and i try to reset PLL2 and PLL3 with the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. store clock registers&lt;/P&gt;&lt;P&gt;2. remap PLL2 clocks to PLL3&lt;/P&gt;&lt;P&gt;3. power down PLL2&lt;/P&gt;&lt;P&gt;4. reintialize PLL2 with PFDs&lt;/P&gt;&lt;P&gt;5. remap PLL3 clocks to PLL2&lt;/P&gt;&lt;P&gt;6. power down PLL3&lt;/P&gt;&lt;P&gt;7. reintialize PLL2 with PFDs&lt;/P&gt;&lt;P&gt;8. restore clock registers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At Step 1 when i switch CBCDR[periph_clk_sel] from PLL2 (528Mhz) to PLL3 (480) Mhz, the system crashes. What can i do to switch AHB and MMDC_CH0 to PLL3?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 15:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352112#M48991</guid>
      <dc:creator>christianbach</dc:creator>
      <dc:date>2014-12-15T15:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: Reset PLL2 and PLL3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352113#M48992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLL2 usually is used for DDR (MMDC module), so if program&lt;/P&gt;&lt;P&gt;runs from DDR, it is not possible to change clock (or source of clock)&lt;/P&gt;&lt;P&gt;of MMDC module. One needs to put DDR to self-refresh, jump to iRAM,&lt;/P&gt;&lt;P&gt;switch/change clocks for MMDC, then return to normal operation from DDR.&lt;/P&gt;&lt;P&gt;In general also crash can be caused by PFD gating, described in&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/eng_bulletin/EB790.pdf?fasp=1&amp;amp;WT_TYPE=Engineering%20Bulletins&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;EB790&lt;/A&gt; Configuration of Phase Fractional Dividers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 00:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352113#M48992</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-16T00:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: Reset PLL2 and PLL3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352114#M48993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 08:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reset-PLL2-and-PLL3/m-p/352114#M48993</guid>
      <dc:creator>christianbach</dc:creator>
      <dc:date>2014-12-16T08:17:26Z</dc:date>
    </item>
  </channel>
</rss>