<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question, i.MX6Q SSI RX by SDMA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351876#M48964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;What is connection scheme between i.MX6 (AUDMUX) and the DSP ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; PTCR2 is configured so, that the DSP (connected to AUD3) should provide&lt;BR /&gt; Receive Frame Sync and Receive Clock : is it so ? Is the DSP configured&lt;BR /&gt; in such mode ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; RXDSEL[2:0] of PDCR2 should be set as 3 (2 in the case) – in order to&lt;BR /&gt; to get data from the DSP via AUD3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Apr 2015 10:01:58 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-04-13T10:01:58Z</dc:date>
    <item>
      <title>Question, i.MX6Q SSI RX by SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351874#M48962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer is facing the issue that the RX from SSI by SDMA does not work on their custom board.&lt;/P&gt;&lt;P&gt;They use SDMA for TX/RX from/to SSI of i.MX6.&lt;/P&gt;&lt;P&gt;TX by SDMA works fine but RX does not work.&lt;/P&gt;&lt;P&gt;They use AUDMUX, SSI2 and AUD3 are used to connect with external DSP.&lt;/P&gt;&lt;P&gt;TXD, RXD,TXFS and TXC pins are used.&lt;/P&gt;&lt;P&gt;The following register dump is captured when the TX completion interrupt occurs.&lt;/P&gt;&lt;P&gt;i.MX6 is expected to receive audio data from external DSP at that time but no data has been received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SSI2_SRX:0x00000000&lt;/P&gt;&lt;P&gt;SSI2_SISR:0x000011e1&lt;/P&gt;&lt;P&gt;SSI2_SCR:0x000000bf&lt;/P&gt;&lt;P&gt;SSI2_SIER:0x005000f&lt;/P&gt;&lt;P&gt;SSI2_STCR:0x000001e9&lt;/P&gt;&lt;P&gt;SSI2_SRCR:0x00000189&lt;/P&gt;&lt;P&gt;SSI2_SFCSR:0x00880788&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AUDMUX&lt;/P&gt;&lt;P&gt;PTCR2:0x94842800&lt;/P&gt;&lt;P&gt;PDCR2:0x00004000&lt;/P&gt;&lt;P&gt;PTCR3:0x8c421800&lt;/P&gt;&lt;P&gt;PDCR3:0x00002000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any ideas about the cause of this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 05:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351874#M48962</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-03-26T05:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q SSI RX by SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351875#M48963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know whether the customer's AUDMUX register settings(&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; line-height: 1.5em;"&gt;PTCR2, &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; line-height: 1.5em;"&gt;PDCR2, &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; line-height: 1.5em;"&gt;PTCR3, &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; line-height: 1.5em;"&gt;PDCR3&lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; line-height: 1.5em;"&gt;) are correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;As I wrote in previous, 4 wires(TXD, RXD, TXFS, TXC) of AUDMUX Port2(SSI2) and Port3(AUD3) are used for connection to external DSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 06:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351875#M48963</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-03-27T06:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q SSI RX by SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351876#M48964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;What is connection scheme between i.MX6 (AUDMUX) and the DSP ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; PTCR2 is configured so, that the DSP (connected to AUD3) should provide&lt;BR /&gt; Receive Frame Sync and Receive Clock : is it so ? Is the DSP configured&lt;BR /&gt; in such mode ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; RXDSEL[2:0] of PDCR2 should be set as 3 (2 in the case) – in order to&lt;BR /&gt; to get data from the DSP via AUD3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2015 10:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-SSI-RX-by-SDMA/m-p/351876#M48964</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-13T10:01:58Z</dc:date>
    </item>
  </channel>
</rss>